Wireless
  • Technologies
  • More
Wireless
Blog Augmenting GPS
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 18 May 2014 6:36 PM Date Created
  • Views 2774 views
  • Likes 0 likes
  • Comments 7 comments
Related
Recommended

Augmenting GPS

gervasi
gervasi
18 May 2014

By 2018 a centimeter-resolution positioning system is scheduled to be in operation covering Japan and locations at the same longitude.  The system will augment the US GPS system. 

 

The satellites will be in geosynchronous (not geostationary) orbit that will cause them to trace a figure eight in the sky over Japan. 

image

The high elevation in the sky increases the number of satellites that will have a direct path to receivers in Japan’s densely populated cities. 

 

The US GPS system uses 1575.42 MHz and 1227.60 MHz.  The centimeter level augmentation signal (CLAS) will be on 1278.75 MHz.  Several ground stations will monitor the location calculated from fixed receivers.  A control center compares the error due to the variable propagation rate of radio waves passing through the ionosphere.  It computes parameters that receivers can use to compensate for this variation and send them to the satellites to be transmitted to QZSS receivers.  The data is compressed and sent at 2kbps to make it more robust.  The process of computing the parameters, compressing them, and getting them to the satellites and back takes six to ten seconds.

 

The system also has a provision for sending text messages to receivers during an emergency when terrestrial communications systems are down.  All references I can find say this information will be carried in the 2 GHz S-band.  If this is in the high-end of 2 GHz, I wonder if receiver manufacturers will choose to omit this feature. 

 

In the 80s and 90s some amateur radio operators secretly hoped for a disaster to take out the phone lines to give amateur operators a chance to provide emergency communications.  I do not know if those people are still around, but it’s hard to imagine amateurs being able to provide communications today in a disaster.  (I didn’t research this claim.  I would love to hear from amateurs involved in emergency preparedness in the comments.)  A simple messaging system that receives messages directly from satellites on mobile phones would be very useful.  My only concern about the system is whether it being on the 2GHz band will make it too costly for high-volume GPS receivers in mobile phones.

 

Conclusion

QZSS approaches the problem of increasing accuracy and coverage by having satellites high in its users’ sky.  This increases the chance of getting a direct path to more than one satellite in an urban environment. 

 

I wonder if anyone has looked into a GPS-augmentation approach based solely on terrestrial transmitters.  The transmitters would be on the users’ horizon instead of in the sky.  Multipath reflections would be much worse, but if the pulses were very short, a good receiver could work out the time of the shortest path, i.e. the first “tap” of the channel function.  The pulse being short, would mean it would have a higher bandwidth and therefore require more power to attain a good SNR at the receiver.  This would not be a problem, though, for a transmitter and antenna located with other repeaters and broadcast stations at a radio tower.

 

Further Reading

  • A nice page on the QZSS website explaining error due to multipath and variable delay in the ionosphere
  • Recent Spectrum article on QZSS
  • A brief comparison of QZSS with other satellite positioning systems
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +2
    You owe the professional community to which you belong and the amateur radio community to which you obviously do not belong an apology. To make the statements you make concerning ham radio operators shows…
  • sqkybeaver
    sqkybeaver over 12 years ago +2
    I confirm that radio amateurs can in fact help with communications in today's emergencies.
  • lairdkelly
    lairdkelly over 12 years ago in reply to e14 Contributor +1
    Professional? Surely you jest... A professional wouldn't sneer at the Amateur Radio community, nor would a professional make a comment like " I wonder if anyone has looked into a GPS-augmentation approach…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    You owe the professional community to which you belong and the amateur radio community to which you obviously do not belong an apology. To make the statements you make concerning ham radio operators shows a dearth of basic knowledge or concern for the truth and is insulting to the hundreds of hams who serve in every major disaster for no reward but to serve. They certainly don't do it to be some kind of twisted heroes. I suggest you refrain from commenting on thing you have admittedly not reasearched.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lairdkelly
    lairdkelly over 12 years ago in reply to e14 Contributor

    Professional? Surely you jest... A professional wouldn't sneer at the Amateur Radio community, nor would a professional make a comment like "I wonder if anyone has looked into a GPS-augmentation approach based solely on terrestrial transmitters..." as a *PROFESSIONAL* would know that it describes LOng Range Aid to Navigation (aka LORAN) which could often be as accurate as GPS (if not more so) but was replaced primarily at the instigation of the US military( because terrestrial transmitters are harder to defend against enemy attack that an orbital satellite transmitter)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • lairdkelly
    lairdkelly over 12 years ago in reply to e14 Contributor

    Professional? Surely you jest... A professional wouldn't sneer at the Amateur Radio community, nor would a professional make a comment like "I wonder if anyone has looked into a GPS-augmentation approach based solely on terrestrial transmitters..." as a *PROFESSIONAL* would know that it describes LOng Range Aid to Navigation (aka LORAN) which could often be as accurate as GPS (if not more so) but was replaced primarily at the instigation of the US military( because terrestrial transmitters are harder to defend against enemy attack that an orbital satellite transmitter)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to lairdkelly

    You are absolutely correct! In fact, as a private pilot, I will also bring up VOR navigation.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gervasi
    gervasi over 12 years ago in reply to lairdkelly

    The nice thing about LORAN was high signal strength.  The signal strength developed on a small GPS antenna is in the -120dBm range.  It amazes me that inexpensive receivers can detect such weak signals.  Regardless of the receiver, it would be easier to jam GPS.

     

    When I was thinking of a terrestrial component, I was thinking of something around urban areas on tall towers in the 1GHz range, so it could easily be integrated with GPS receivers operating in the same frequency range. Range would be line-of-sight (unlike LORAN in the 100kHz range) so it would have to be deployed in urban areas or maybe a temporary setup in a war zone.