Wireless
  • Technologies
  • More
Wireless
Blog Testing HD Radio
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gervasi
  • Date Created: 19 Jul 2013 11:49 PM Date Created
  • Views 1715 views
  • Likes 2 likes
  • Comments 6 comments
  • hd_radio
Related
Recommended

Testing HD Radio

gervasi
gervasi
19 Jul 2013

A few months ago someone asked me where to find an HD radio.  Despite my interest in radio, I had heard of HD but knew almost nothing about it. 

 

When I researched it, I learned that digital broadcasting (as expected) is much more efficient, but no digital standard has been adopted to replace AM/FM broadcast radio.  “HD radio” is the digital standard the US adopted. 

 

HD originally stood for hybrid-digital because the signals are transmitted in parallel with the legacy analog transmissions.  HD is now just the brand name for the standard.  It has never stood for high-definition. 

 

High-performance radio retailer CCrane told me they have plans no to carry an HD radio.  They tried many models and could not find a single receiver that met their standards.  They said, "AM reception is abominable on all of the HD tuners we tested".  When they did carry them the return rate was two to three times the rate for other radios.  This is possibly because the subcarrier that carries HD is 20dB down from the analog carrier, so you need a strong signal to receive HD reliably. 

 

Testing Insignia NS-HDRADimage

I tested the Insignia NS-HDRAD receiver.  It did very well.  There was no noticeable intermodulation from the strong FM stations located near the office.  It detected the HD signal from several stations in my area. 

 

Most stations with HD provide two channels with similar programming.  The WI Public Radio FM station in my area has three choices of digital programming on the same frequency.  Their third subchannel is dedicated to talk programming and had noticeably limited audio bandwidth.  Stations can have several subchannels, but at least one must be at least the same quality as the analog signal .

 

One nice feature with the Insignia radio is the AUX IN port.  I used it to listen to audio from my MP3 player.

 

The biggest downside to this radio is it has no AM coverage.  I looked at other HD radios, and many have no AM or analog-only AM. 

 

Another issue is the volume.  I had to turn up the volume near maximum to listen to the low-bandwidth digital station with talk programming.  The same was true when listening to my MP3 player (at its max volume) through the AUX port. 

 

Next Time

Next week I test a JVC KT-HDP1, which does support AM, and tear it down.  It becomes clear that someone needs to design a high-quality AM/FM HD Radio receiver.

  • Sign in to reply
Parents
  • sqkybeaver
    sqkybeaver over 13 years ago

    while digital portion is usually -20dB from the fm portion and uses less bandwidth than traditional fm, the digital signal just about doubles the total used bandwidth to 400KHz. I don't think that it is that efficent, It also means you can't have stations as close as fm-only stations could be(both in frequency and geographically)

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to sqkybeaver

    In the UK at least, many consumer radios have poor AM, but many also have poor analog FM although some would argue it is still preferable to DAB (Digital Audio Broadcasting) in realistic scenarios (I'd have to agree with that, in the area where I live). Analog FM can sound extremely good, but requires (expensive) analog filters and circuits. Modern FM circuits are designed to optimize out the number of analog sections (to reduce BoM cost, but also to optimize the number of alignments/adjustments down to zero) which isn't the same as optimizing for sound quality :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gervasi
    gervasi over 13 years ago in reply to shabaz

    Thanks for the UK perspective.  I've never been there.  Here most FM radios tune in 200kHz increments (not 100kHz as in Europe).  They generally sound good on good speakers or headphones but they have horrible dynamic range.  If you're in a mid-sized city anywhere near a couple transmitters, you'll hear intermod from the strong transmitters all over the band.  Where I live there are two stations two or three km south of me, and I hear them all around the band.  "What's this station I didn't know about at 93MHz?  Oh thats, 104.1MHz."  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to gervasi

    Hi Gervasi, I think you're right, some countries squash many stations in. The SNR is awful on some radios, and one can't tell (at least, not in a store) if it is due to the design of it, or due to the interference from the rest of the stations. I guess it is a combination of both, and good filtering on the input is expensive. Plus, radios are one of those things which really are end-to-end where just one part of the design can make or destroy the end result, so someone making a design (or cost) decision in any part of the radio will affect the entire result.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 13 years ago in reply to gervasi

    Hi Gervasi, I think you're right, some countries squash many stations in. The SNR is awful on some radios, and one can't tell (at least, not in a store) if it is due to the design of it, or due to the interference from the rest of the stations. I guess it is a combination of both, and good filtering on the input is expensive. Plus, radios are one of those things which really are end-to-end where just one part of the design can make or destroy the end result, so someone making a design (or cost) decision in any part of the radio will affect the entire result.