Wireless
  • Technologies
  • More
Wireless
Forum Cheap 433MHz ASK modules in commercial applications. Pros and Cons
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 219 subscribers
  • Views 4062 views
  • Users 0 members are here
  • ip_iot
  • sub-ghz
  • 433 mhz
  • rf communication
Related

Cheap 433MHz ASK modules in commercial applications. Pros and Cons

ipv1
ipv1 over 5 years ago

Hi all,

 

I am working on some short range RF sensors that include contact and ADC information. The data is transmitted to a nearby hub/aggregator but the sensor nodes themselves are battery driven and must be lower cost.

 

I have dissected a few door sensors on ebay and amazon and they seem to use 433MHz ASK modules that are quite cheap, albeit, one way and dumb. I understand that logic and flow control must be added externally via a microcontroller/processor but the real question here is...

 

"Should/Can we use 433MHz for commercial applications?"

 

LoRa is a better but a slightly costlier option. There are other Sub-GHz modules out there but they are more difficult to create small batches with.

 

Inputs on the 433MHz module use and suggestions are warranted here.

 

Thanks,

 

IP

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +4
    433MHz can do FSK as well. There are lots of commercial applications for 433MHz, but I think there are restrictions on the amount of data and air time, so if you are monitoring continuously, there may…
  • BigG
    BigG over 5 years ago +3
    "Should/Can we use 433MHz for commercial applications?" IMHO this is mature tech. I recall 433MHz keyfobs, for example, back in the late 1990's. These would've used Manchester encoding and used proprietary…
  • shabaz
    shabaz over 5 years ago +2
    Hi Inderpreet, Depending on your needs, you might find you can't do as much with the 433 MHz modules. The cheap modules can drift a lot, and can't offer multiple channels as easily, since they are not…
Parents
  • BigG
    BigG over 5 years ago

    "Should/Can we use 433MHz for commercial applications?" IMHO this is mature tech.

     

    I recall 433MHz keyfobs, for example, back in the late 1990's. These would've used Manchester encoding and used proprietary protocols and methodologies to allow the user to link a keyfob with a particular receiver. It was all closed shop... and that's the rub.

     

    In my experience, I have found no open source or standardised/proven methods and additional middleware to handle data security etc. and how to link a particular transmitter with a particular receiver. This part you have to do/create yourself. Probably by now there is stuff on the internet but it is nothing standardised or elaborate like LoRa or BLE.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 5 years ago

    "Should/Can we use 433MHz for commercial applications?" IMHO this is mature tech.

     

    I recall 433MHz keyfobs, for example, back in the late 1990's. These would've used Manchester encoding and used proprietary protocols and methodologies to allow the user to link a keyfob with a particular receiver. It was all closed shop... and that's the rub.

     

    In my experience, I have found no open source or standardised/proven methods and additional middleware to handle data security etc. and how to link a particular transmitter with a particular receiver. This part you have to do/create yourself. Probably by now there is stuff on the internet but it is nothing standardised or elaborate like LoRa or BLE.

    • Cancel
    • Vote Up +3 Vote Down