Wireless
  • Technologies
  • More
Wireless
Forum Cheap 433MHz ASK modules in commercial applications. Pros and Cons
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 219 subscribers
  • Views 4069 views
  • Users 0 members are here
  • ip_iot
  • sub-ghz
  • 433 mhz
  • rf communication
Related

Cheap 433MHz ASK modules in commercial applications. Pros and Cons

ipv1
ipv1 over 5 years ago

Hi all,

 

I am working on some short range RF sensors that include contact and ADC information. The data is transmitted to a nearby hub/aggregator but the sensor nodes themselves are battery driven and must be lower cost.

 

I have dissected a few door sensors on ebay and amazon and they seem to use 433MHz ASK modules that are quite cheap, albeit, one way and dumb. I understand that logic and flow control must be added externally via a microcontroller/processor but the real question here is...

 

"Should/Can we use 433MHz for commercial applications?"

 

LoRa is a better but a slightly costlier option. There are other Sub-GHz modules out there but they are more difficult to create small batches with.

 

Inputs on the 433MHz module use and suggestions are warranted here.

 

Thanks,

 

IP

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +4
    433MHz can do FSK as well. There are lots of commercial applications for 433MHz, but I think there are restrictions on the amount of data and air time, so if you are monitoring continuously, there may…
  • BigG
    BigG over 5 years ago +3
    "Should/Can we use 433MHz for commercial applications?" IMHO this is mature tech. I recall 433MHz keyfobs, for example, back in the late 1990's. These would've used Manchester encoding and used proprietary…
  • shabaz
    shabaz over 5 years ago +2
    Hi Inderpreet, Depending on your needs, you might find you can't do as much with the 433 MHz modules. The cheap modules can drift a lot, and can't offer multiple channels as easily, since they are not…
Parents
  • shabaz
    shabaz over 5 years ago

    Hi Inderpreet,

     

    Depending on your needs, you might find you can't do as much with the 433 MHz modules. The cheap modules can drift a lot, and can't offer multiple channels as easily, since they are not designed to channel hop. Personally I would be looking at other sub-GHz models, or as BigG says, BLE or some other 2.4 GHz protocol. There's commercial stuff using proprietary 2.4 GHz protocols too. Also Zigbee can be popular for certain industries, perhaps chosen because on paper it has a security layer although it's optional from memory. 

    Consumer stuff still uses 433 MHz ASK modules, but sometimes it's dated designs (not because of the chosen frequency of course, but because perhaps radio wasn't a core area of expertise for the manufacturer. I think my home heating system uses such a module, and it's a pretty poor designed solution.

    If you're designing a consumer solution then perhaps it may be the cheapest option admittedly, simply because it's so mature.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 5 years ago

    Hi Inderpreet,

     

    Depending on your needs, you might find you can't do as much with the 433 MHz modules. The cheap modules can drift a lot, and can't offer multiple channels as easily, since they are not designed to channel hop. Personally I would be looking at other sub-GHz models, or as BigG says, BLE or some other 2.4 GHz protocol. There's commercial stuff using proprietary 2.4 GHz protocols too. Also Zigbee can be popular for certain industries, perhaps chosen because on paper it has a security layer although it's optional from memory. 

    Consumer stuff still uses 433 MHz ASK modules, but sometimes it's dated designs (not because of the chosen frequency of course, but because perhaps radio wasn't a core area of expertise for the manufacturer. I think my home heating system uses such a module, and it's a pretty poor designed solution.

    If you're designing a consumer solution then perhaps it may be the cheapest option admittedly, simply because it's so mature.