Wireless
  • Technologies
  • More
Wireless
Forum project. need help and advice from all the expert here .
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 219 subscribers
  • Views 838 views
  • Users 0 members are here
Related

project. need help and advice from all the expert here .

e14 Contributor
e14 Contributor over 16 years ago

hi,

 

 

im a student and currently i am doing a project in a hospital to remind everyone to wash their hands, my group came up with 2 ideas, RFID and/or sensors which is integrated with the hand rub which act as a switch to verify hand rub have been done.

 

firstly,

 

 

 

RFID,we could not figure out how much is would cost and how it works. it is because we need to ensure EVERY staff to wash their hands as these doctors tends to forgot and did not bother to wash their hands, and also in the other hand, we want everyone to do also as there are also visitors. cost is an issue and RF might affect the patient health? and is the programming long?

 

 

 

sensor, we could not figure out how to place the sensors as there will be people moving around and could not determine if the person has already washed their hand. but sensors are much cheaper comparing to the RFID..

 

need ideas and advice from everyone here.. i really could not think of other way to deal with the sensors.. please help me!

 

thank you for reading image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi,

     

    Usually in hospitals 868MHz and 2.4GHz ranges are approved for usage.

    This taken into consideration UHF passive RFID tags could be used but the readers are expensive.

     

    Tags can be cheap but the readers and the reading range can be an issue if you need to keep the cost low.

     

    Hopefully this helps at least a bit.

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 16 years ago

    Hi,

     

    Usually in hospitals 868MHz and 2.4GHz ranges are approved for usage.

    This taken into consideration UHF passive RFID tags could be used but the readers are expensive.

     

    Tags can be cheap but the readers and the reading range can be an issue if you need to keep the cost low.

     

    Hopefully this helps at least a bit.

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor
    thanks for the reply..!
    yes it helped.. maybe sensors are the only way to do it.. just need to position the sensors  image

     

    what is the price range by the way?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    UHF readers are usually available from around 300€ upwards, depending on the reading range and type of a reader.

     

    Cheapest RFID readers (starting from around 70€ or something like that) are available for 125kHz passive tags but the read range is only some centimeters and the required antennas for more range need to be very large (eg. 60cm).

     

    If you also want the sensor data to be used in some way you would need a custom RF solution or possibly to hook into an existing WLAN/ethernet in the hospital.

     

     

    Elias