Wireless
  • Technologies
  • More
Wireless
Forum Material to absorb RF
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 221 subscribers
  • Views 4896 views
  • Users 0 members are here
Related

Material to absorb RF

skeevestevens
skeevestevens over 8 years ago

I need to put an antenna close to/against metal.

 

What sort of material could I put below it to absorb the RF rather than the metal reflecting it?

 

...Skeeve

  • Sign in to reply
  • Cancel

Top Replies

  • gervasi
    gervasi over 8 years ago +2 suggested
    What are you trying to accomplish? Ordinarily I'm trying to prevent objects near an antenna from absorbing energy from the antenna. Once you tell me your goal, I may realize I was missing an obvious inference…
  • skeevestevens
    skeevestevens over 8 years ago in reply to gervasi +1
    Hey Charles, I have a big metal box 1m3 with no top. I have a reader under the box with a small hole in the corner for the antenna to pop through and be in the very corner due to the volatile nature of…
  • gervasi
    gervasi over 8 years ago in reply to skeevestevens +1 suggested
    The antenna will be right against steel and aluminium. The antenna will be right against steel and aluminium. I think you should have the antenna not contact the aluminum, but it can be close. If possible…
Parents
  • jc2048
    0 jc2048 over 8 years ago

    If it's microwave (2.4GHz ISM or above) you might consider a patch antenna. That could sit against metal without any problems (internally, the patch is placed just above a ground plane, so further metal underneath doesn't affect the properties). You can buy commercial patch antennas with ceramic between the patch and the plane. Here's an example (not a recommendation - I've never used one of these)

     

    http://www.taoglas.com/product/wlp-2450-25-4-a-02-2-4ghz-bluetooth-wlan-zigbee-patch-antenna-25mm/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 8 years ago

    If it's microwave (2.4GHz ISM or above) you might consider a patch antenna. That could sit against metal without any problems (internally, the patch is placed just above a ground plane, so further metal underneath doesn't affect the properties). You can buy commercial patch antennas with ceramic between the patch and the plane. Here's an example (not a recommendation - I've never used one of these)

     

    http://www.taoglas.com/product/wlp-2450-25-4-a-02-2-4ghz-bluetooth-wlan-zigbee-patch-antenna-25mm/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer