Wireless
  • Technologies
  • More
Wireless
Forum How to transmit data underwater over 40m
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 13 answers
  • Subscribers 225 subscribers
  • Views 12725 views
  • Users 0 members are here
  • data communication
  • wireless_transfer
  • underwater
  • radio communications
  • ultra sound
  • accoustic
Related

How to transmit data underwater over 40m

ahenon
ahenon over 6 years ago

Dear All,

 

I would need to transmit data in salted water in both ways on a distance of 40 to 50 meters maximum with no cable.

The quantity of data is not important only constarint is to use to much energy and not to expensive. Apparently the best option would be ultrasound:

 

I found some interesting device on internet:

http://www.benthowave.com/products/BII-7520omnidirectionaltransducer.html

 

As I'm a mechanical engineer, I have no clue on which material I should buy to test underwater data transmission...

 

So I have 3 Questions:

 

1/ Is the ultra sound option the only one for my application, if not, what do you recommand ?

2/ In the case of ultrasound communication, which reference of equipment should I buy (maybe in the link I gave before or you have better options?)

3/ If you think of other options than ultrasound, do you have any reference of electronic system I should buy for testing?

 

Thanks a lot,

 

Alexandre

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +4 suggested
    There are a couple of points in your responses to Doug's questions that need some more detail. 7 - Data rate - I'm not sure what units o/s are but let's assume it to be 10 x 64 bit words per second - you…
  • jw0752
    jw0752 over 6 years ago +3 suggested
    Hi Alexandre, If a low data rate is permissible you might find that you can get more distance with less power by using a lower frequency carrier. Infra-sound would carry greater distance as it is less…
  • dougw
    dougw over 6 years ago +3 suggested
    How large can the communication system be? How much power is available? Is the water turbulent? Is the water clear or murky? Are there any obstacles in the water? (Is it a straight line-of-sight)? Is there…
Parents
  • neuromodulator
    0 neuromodulator over 6 years ago

    Alternatives are, radiofrequency,  Light and sound.

     

    RF has a pretty hard time penetrating salty water, and you require very low frequencies. Laser can get longer distances, but it has to be aimed and still won't go much farther than RF. Then ultrasound can get to very long distances, many kms if needed, but there is always the tradeoff of range and rate. And still ultrasound will always have limited latency, because of speed of sound in water.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • neuromodulator
    0 neuromodulator over 6 years ago

    Alternatives are, radiofrequency,  Light and sound.

     

    RF has a pretty hard time penetrating salty water, and you require very low frequencies. Laser can get longer distances, but it has to be aimed and still won't go much farther than RF. Then ultrasound can get to very long distances, many kms if needed, but there is always the tradeoff of range and rate. And still ultrasound will always have limited latency, because of speed of sound in water.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer