Wireless
  • Technologies
  • More
Wireless
Forum How to transmit data underwater over 40m
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 13 answers
  • Subscribers 225 subscribers
  • Views 12725 views
  • Users 0 members are here
  • data communication
  • wireless_transfer
  • underwater
  • radio communications
  • ultra sound
  • accoustic
Related

How to transmit data underwater over 40m

ahenon
ahenon over 6 years ago

Dear All,

 

I would need to transmit data in salted water in both ways on a distance of 40 to 50 meters maximum with no cable.

The quantity of data is not important only constarint is to use to much energy and not to expensive. Apparently the best option would be ultrasound:

 

I found some interesting device on internet:

http://www.benthowave.com/products/BII-7520omnidirectionaltransducer.html

 

As I'm a mechanical engineer, I have no clue on which material I should buy to test underwater data transmission...

 

So I have 3 Questions:

 

1/ Is the ultra sound option the only one for my application, if not, what do you recommand ?

2/ In the case of ultrasound communication, which reference of equipment should I buy (maybe in the link I gave before or you have better options?)

3/ If you think of other options than ultrasound, do you have any reference of electronic system I should buy for testing?

 

Thanks a lot,

 

Alexandre

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 6 years ago +4 suggested
    There are a couple of points in your responses to Doug's questions that need some more detail. 7 - Data rate - I'm not sure what units o/s are but let's assume it to be 10 x 64 bit words per second - you…
  • jw0752
    jw0752 over 6 years ago +3 suggested
    Hi Alexandre, If a low data rate is permissible you might find that you can get more distance with less power by using a lower frequency carrier. Infra-sound would carry greater distance as it is less…
  • dougw
    dougw over 6 years ago +3 suggested
    How large can the communication system be? How much power is available? Is the water turbulent? Is the water clear or murky? Are there any obstacles in the water? (Is it a straight line-of-sight)? Is there…
Parents
  • dougw
    0 dougw over 6 years ago
    1. How large can the communication system be?
    2. How much power is available?
    3. Is the water turbulent?
    4. Is the water clear or murky?
    5. Are there any obstacles in the water? (Is it a straight line-of-sight)?
    6. Is there marine life that cannot be disturbed?
    7. What data rate is adequate?
    8. How deep is it?
    9. Can an antenna stick out of the water?
    10. Is there movement of one or both ends of the link?
    11. Does the link need to be omni-directional?
    12. Does the communication need to be real-time? (could a robot go back and forth?)
    13. What is the cost target?
    14. How much time is available for development?

    There are a large number of answers to your question, including the technologies mentioned in other responses above and commercial communication systems and a couple of others I can think of, but if you want to narrow it down to a solution that works well for you, it would help to try to answer these questions.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ahenon
    0 ahenon over 6 years ago in reply to dougw

    Hello Doug,

     

    Thanks a lot for your questions, please find my answers below:

    1. How large can the communication system be? 10x10x20 cm each
    2. How much power is available? enough to transmit data during 48hrs -> see data rate
    3. Is the water turbulent? There can be 3 knots/hr stream
    4. Is the water clear or murky? Murky
    5. Are there any obstacles in the water? (Is it a straight line-of-sight)? No obstacle
    6. Is there marine life that cannot be disturbed? No
    7. What data rate is adequate? 10 o/s
    8. How deep is it? 25 meters max
    9. Can an antenna stick out of the water? No
    10. Is there movement of one or both ends of the link? yes on one end
    11. Does the link need to be omni-directional? Yes
    12. Does the communication need to be real-time? (could a robot go back and forth?) Real time
    13. What is the cost target? from 30$ or 100$ max (minimum is the best)
    14. How much time is available for development? 6 months to 12 months

     

    So do you see any options?

     

    Thanks a lot for your help,

     

    Alexandre

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 6 years ago in reply to ahenon

    In this situation, I would likely try FSK between 2 different waterproof ultrasonic transducers to reduce multipath ambiguity.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 6 years ago in reply to ahenon

    In this situation, I would likely try FSK between 2 different waterproof ultrasonic transducers to reduce multipath ambiguity.