Wireless
  • Technologies
  • More
Wireless
Forum Zigbee...ginner "Zigbee or not Zigbee" that is the question...
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 219 subscribers
  • Views 937 views
  • Users 0 members are here
  • short-range
  • zigbee
Related

Zigbee...ginner "Zigbee or not Zigbee" that is the question...

e14 Contributor
e14 Contributor over 16 years ago
My question is so stupid i am ashamed to post it but it is too late. My intention is to add voice fonction and perhaps low quality vidéo to a portable product. Can Zigbee be (lol) the right product? What will be the range with a short antenna or even a long one? 100 meters ?
  • Sign in to reply
  • Cancel
Parents
  • wendydu
    0 wendydu over 16 years ago

    Hello, I'm afraid zigbee is not suitable for video but maybe control application doesn't need high speed. Zigbee is low cost low power wireless networking standard and the speed rate is not so high: 250 kbit/s per channel in the 2.4 GHz band, 40 kbit/s per channel in the 915 MHz band, and 20 kbit/s in the 868 MHz band. So you may consider what speed you in this application, do you mean that real time vedio transmit or just for downloading data?  Also the transmission range you should consider it: transmission range is between 10 and 75 meter (33 and 246 feet) and up to 1500 meters.

     

    Beside, the antenna size is according to the operating frequency. In general antenna size decreases with increase in frequency, and the antenna size could be similar to the wave length or longer or shorter, depend on the type and performance of the antenna. For Zigbee, the antenna size could be several mm to hundred mm, you can choose PCB antenna, chip antenna or whip antenna for you design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to wendydu

    Thanks for your quick reply and i think i will spend a little more of your time. What will be the best technology for me?

    I really need to transmit real time images at low quality as a small webcam from a GSM for example. For the speed

    it can be ok even with a little lag. When you say "up to 1500 meters" it is huge and very tempting. Do you have an example of

    realization? .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wendydu
    0 wendydu over 16 years ago in reply to e14 Contributor

    Does this design use to apply CCTV system or something like that?

    If it use to do that, maybe you can choose bluetooth if you don't need long range.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 16 years ago in reply to wendydu
    In fact yes but on a long range. I didn't know that Bluetooth has a long range.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wendydu
    0 wendydu over 16 years ago in reply to e14 Contributor
    No, Bluetooth didn't have a long range so you need to set up a network by using bluetooth
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wendydu
    0 wendydu over 16 years ago in reply to e14 Contributor
    No, Bluetooth didn't have a long range so you need to set up a network by using bluetooth