Wireless
  • Technologies
  • More
Wireless
Forum GPS modem interfacing with controllers
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 13 replies
  • Answers 1 answer
  • Subscribers 220 subscribers
  • Views 2458 views
  • Users 0 members are here
Related

GPS modem interfacing with controllers

e14 Contributor
e14 Contributor over 16 years ago

Hi,

 

I am a student and I plan on making a final year project. I am trying to connect a controller to a mobile device using a wireless connection. I have no ideea what kind of wireless module to use. Are there some kind of GPS modems that can do this task? I am planning on transfering large data if possible. Maybe a GPRS or EDGE connection can be realized some how.

I have also heard about some long distance wireless kits ( can go up to 7km). Can these be connected to my smartphone/PDA?I know these are using 802.15 protocol while the phone WiFi is 802.11g.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Sorry for the late entry, but this can be done pretty cheaply.  Here's how.

     

    First, you can pick up a SIM900D GSM/GPRS cell module for under $30US.  Any GSM/GPRS module will work because they all use the same AT commands.

     

    Next, you can use a small microcontroller to grab the data from the GPS module and use the built in TCP/IP stack in the modem to send it anywhere you want.

     

    Optionally, if you don't want to mess with the microcontroller, you can use a chip from ConnectOne.  The made TCP/IP routing engines for embedded apps.  Simply connect the GPS device to a serial port, configure the CO chip as a SerialNET device, connect the modem to another port and you are good to go.  The SerialNET mode will basically open a TCP connection to an IP address you choose and send any data from the GPS serial port to that address as streaming bytes.

     

    In the end, you spend $30 on the GPRS module, $38 on a pre-packaged ConnectOne module (based on the CO2128 chip, you can buy them from Mouser), and $30 on a GPS module.  The total cost is $98US or 70 Euros.  Not bad.

     

    I am current working on a project using all of these devices and would be more than happy to help if I can.

     

    Regards,

     

    Steve The RF Guy

    God Bless the USA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Sorry for the late entry, but this can be done pretty cheaply.  Here's how.

     

    First, you can pick up a SIM900D GSM/GPRS cell module for under $30US.  Any GSM/GPRS module will work because they all use the same AT commands.

     

    Next, you can use a small microcontroller to grab the data from the GPS module and use the built in TCP/IP stack in the modem to send it anywhere you want.

     

    Optionally, if you don't want to mess with the microcontroller, you can use a chip from ConnectOne.  The made TCP/IP routing engines for embedded apps.  Simply connect the GPS device to a serial port, configure the CO chip as a SerialNET device, connect the modem to another port and you are good to go.  The SerialNET mode will basically open a TCP connection to an IP address you choose and send any data from the GPS serial port to that address as streaming bytes.

     

    In the end, you spend $30 on the GPRS module, $38 on a pre-packaged ConnectOne module (based on the CO2128 chip, you can buy them from Mouser), and $30 on a GPS module.  The total cost is $98US or 70 Euros.  Not bad.

     

    I am current working on a project using all of these devices and would be more than happy to help if I can.

     

    Regards,

     

    Steve The RF Guy

    God Bless the USA