Wireless
  • Technologies
  • More
Wireless
Forum HELP: How to link multiply transmitter to one receiver
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 219 subscribers
  • Views 1920 views
  • Users 0 members are here
  • rf_design_engineer
  • wireless
  • rf
  • internal_wireless_connection
  • wireless_lab
Related

HELP: How to link multiply transmitter to one receiver

e14 Contributor
e14 Contributor over 15 years ago

Hi all, I would like to ask how can i link seven Transmitter to one receiver. I am using QFM-TX1-433 as my transmitter and QFM-RX1-433 as my receiver and also RF803E for the rf encoder, RF803D for the rf decoder. Currently I am able to link one transmitter to the receiver individually. It works perfectly when i operate one transmitter at one time, but when i operate more than one transmitter, the receiver can only able to detect one transmitter at most. I am just sending one digital signal. I had used the same input for the encoder but configured differently at the output of the decoder for every encoder. I would like ask is it I had used the wrong rf transmitter and receiver, or I had done wrong in the connection. The circuit is about the same as the one in the datasheet, just that I did not include the serial port, I just used all the outputs from the decoder. Thanks alots in advance.

Attachments:
imageDS803-6.pdf
image82797.pdf
image33558.pdf
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Hi

     

    IMHO you will have to time multiplex them (i,e only onw switched on at a time) , they will not work together at the same time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor
    So, it mean that I cannot operate all at the same time? I only want them to be detectable by the receiver when all transmitter is on, because currently my receiver can only detect one particular transmitter and the rest is not detectable at all when they are on at the same time. I will only press one switch at a time, as for the receiver, because I just want it to detect which transmitter is being triggered. I am using one switch for one transmitter.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    If the transmitter sends only when the button is pressed and two buttons are not pressed at the same time, it should work without any gimmicks.

     

    If there is a chance that two buttons are pressed at the same time the transmitter would have to be timed individually to not send at the same "time-slot".

     

     

     

    Elias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor
    I only press one switch at a time, but the receiver can only detect a particular transmitter and the other just not able to be detect. Is it because i had use wrong component?
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Chris_Pinter
    0 Chris_Pinter over 15 years ago in reply to e14 Contributor

    Hello,

     

    This is a normal part of designing radio systems.  Most if not all radio systems have to deal with multiply transmitters. If you are having problems sending a signal from one transmitter to the receiver while the other six units are turned on it is likely that the transmitters are transmitting beckon packets without your knowledge.

     

    You will need to look at the firmware of the transmitter and receiver and develop a method of synchronizing the transmitters so they do not step on each other. Instead of developing the firmware yourself you might be able to get some help from the manufacturer of the radio modules.  They might have provided a patch or a method of synchronizing the transmitters within the development firmware.   I would give them a call first.

     

    If you need help with firmware design I would suggest you consider a simple multiplexing algorithm that incorporates Aloha protocol.  This will solve the next problem you will face, which is an increase in packet errors due to heavy traffic on the channel.

     

    Hope this helps,

     

    Chris

     

    http://www.pinterec.ca/services/wireless-development

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Chris_Pinter
    0 Chris_Pinter over 15 years ago in reply to e14 Contributor

    Hello,

     

    This is a normal part of designing radio systems.  Most if not all radio systems have to deal with multiply transmitters. If you are having problems sending a signal from one transmitter to the receiver while the other six units are turned on it is likely that the transmitters are transmitting beckon packets without your knowledge.

     

    You will need to look at the firmware of the transmitter and receiver and develop a method of synchronizing the transmitters so they do not step on each other. Instead of developing the firmware yourself you might be able to get some help from the manufacturer of the radio modules.  They might have provided a patch or a method of synchronizing the transmitters within the development firmware.   I would give them a call first.

     

    If you need help with firmware design I would suggest you consider a simple multiplexing algorithm that incorporates Aloha protocol.  This will solve the next problem you will face, which is an increase in packet errors due to heavy traffic on the channel.

     

    Hope this helps,

     

    Chris

     

    http://www.pinterec.ca/services/wireless-development