Wireless
  • Technologies
  • More
Wireless
Forum Materials for wideband transformer wanted
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 218 subscribers
  • Views 365 views
  • Users 0 members are here
Related

Materials for wideband transformer wanted

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I need a suitable core for a 80 MHz more or less lossless  transformer where the primary winding is stationary and the secondary winding is rotating with respect to the primary. Maximum power transferred is approx. 10 mW. The impedance must be 50 ohms.

 

Actually two halves of pot-core type of ferrite would be suitable because I must have a minimum 6 mm diameter hole in the center (in the axis of the rotation to be used for a rotating fiber-coupling).

 

I need only 10 pcs. for a special version of one of our instrumentation systems - and all the ferrite I can find out there (with short delivery time) is dedicated

for EMC purposes (noise filtering etc.) and has a lot of losses at 80 MHz (which is fine for EMC purposes - but certainly not for my application).

 

Any suggestions out there?

 

Best regards

Morten Hammer

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 14 years ago

    Hi Morten,

     

    One vendor may be Amidon, they have online ordering. However, at 80MHz, maybe it is only possible to have a wideband transformer using the transmission line transformer (TLT) method? But that would not have a movable winding, because it needs a transmission line design for the wire pairs.

    However, I'm no expert in this area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 14 years ago

    Hi Morten,

     

    One vendor may be Amidon, they have online ordering. However, at 80MHz, maybe it is only possible to have a wideband transformer using the transmission line transformer (TLT) method? But that would not have a movable winding, because it needs a transmission line design for the wire pairs.

    However, I'm no expert in this area.