Wireless
  • Technologies
  • More
Wireless
Forum Power after your done
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 219 subscribers
  • Views 639 views
  • Users 0 members are here
Related

Power after your done

e14 Contributor
e14 Contributor over 13 years ago

I have just finished my first project.  So I thought I would watch the fruits of my labor. I was told that I could plug in a 5v transformer a d the chip would remember my skit and start working.

Well I plugged it in and the LEDs on the UNO lit up but nothing else happened. I unplugged the transformed and plugged the computer back in.  I thought I would reload the program. But before I even opened the program it started working.

Can I use the UNO without a computer or am I tethered for life?

  • Sign in to reply
  • Cancel
  • Catwell
    0 Catwell over 13 years ago

    Are you powering it off of a computer USB port?

    If so, that might be where your power issues are. Although a PC USB port is supposed to supply 5V @ 500mA, it might be sharing that power with other peripherals.

     

    I recommend getting an external 5V power supply, like one for a cell phone. Find some USB to USB adapters to get to the right connector size.

     

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Catwell

    Sorry to kill your suggestion but you have it backwards.  It works fine when I use the computer USB port.  It's when I hook it up to a 5 v power supply that doesn't work.  I was told I might need 9v.  And to use a 9v transformer battery.  Is that true or will I let the smoke out of my arduino?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 13 years ago in reply to e14 Contributor

    I see. Thanks for clearing it up.

     

    Yes, you need a higher voltage. The UNO can take 7 to 12V, recommended. So, 9V should work just fine (around 400mA or more).

    Again, find a power supply that can handle it. They are plentiful.

     

    C