Wireless
  • Technologies
  • More
Wireless
Forum RF Power Amplifier
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 219 subscribers
  • Views 622 views
  • Users 0 members are here
Related

RF Power Amplifier

e14 Contributor
e14 Contributor over 13 years ago

Hi All ,

 

Being an FPGA Design Engineer i have limited insight into RF Circuits and how they behave , i am trying to increase the range of a RF Transciever build around CC430F6137 by using a RF Power Amplifier .

 

But i am not sure how to connect it , the RF output of CC430 is differential and then TI recommends a Balun CKT infront of it and it terminates on a Antenna .

 

The RF Power Amplifier only takes in single input and single output , should i connect the PA after the Balun CKT ???

 

Please see the diagram attached .

 

Thanking you ,

 

 

Ahmed AsimGhouri

FPGA Design Engineer

Tulwar Technologies (pvt) ltd

Website : www.tulwartechnologies.com

Email : info@tulwartechnologies.com

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 13 years ago

    If the circuit is a transceiver (and not a transmitter) then it is not possible to just connect an amplifier. You need some switching capability, often achieved by biasing special diodes. See here (PDF) . However this requires the ability to know when the transceiver is transmitting, so that the switching can be invoked. You may be better off asking the manufacturer (TI) directly for recommendations. You can't just use relays by the way (well, you could, but they

    would be very expensive relays).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    OK, then lets say i just want to transmit for now , referring to the diagram attached can i connect the PA like this ?

    And do i still have to add a impledence matching CKT before antenna ?

     

    For Tx/Rx switching i am considering RF6504

     

    The PA's i am considering is RF5110G

     

    Thanks

     

    Ahmed AsimGhouri

    FPGA Design Engineer

    Tulwar Technologies (pvt) ltd

    Website : www.tulwartechnologies.com

    Email : info@tulwartechnologies.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to shabaz

    OK, then lets say i just want to transmit for now , referring to the diagram attached can i connect the PA like this ?

    And do i still have to add a impledence matching CKT before antenna ?

     

    For Tx/Rx switching i am considering RF6504

     

    The PA's i am considering is RF5110G

     

    Thanks

     

    Ahmed AsimGhouri

    FPGA Design Engineer

    Tulwar Technologies (pvt) ltd

    Website : www.tulwartechnologies.com

    Email : info@tulwartechnologies.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    It's fine as long as you can control your CC430 device (which I'm not familiar with, hence the strong recommendation that you direct your question to TI) to output at a level which won't overload the PA (1dBm level max or thereabouts). You will likely need to do impedance matching, which can be accomplished in a variety of ways, e.g. a network or wideband matching with a transformer. The matching is required if the CC430 impedance is different to the PA.