Wireless
  • Technologies
  • More
Wireless
Forum Discover WIFI SN8200 programming via jtag
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 219 subscribers
  • Views 855 views
  • Users 0 members are here
  • wi-fi
  • wireless
Related

Discover WIFI SN8200 programming via jtag

e14 Contributor
e14 Contributor over 12 years ago

I hope somebody can help with this. I noticed that a previous question went unanswered on the same topic! I have tried to reprogram the stm32f103 uC which is part of the sn8200. The method I used was using uVision4 and ulink2. The bin file that I used came with the software package that can be downloaded from element14 after buying the Discover WIFI module SN8200-SNIC-UART-02.31311.bin. In the first instance trying to flash the module uvision gave an error, so I converted the file to hex using bin2hex. This also gave an error about not having the correct flash driver, so I converted the file again with an offset of 0x08000000 and used the driver that started flashing at 0x00000000. Uvision reported erasing the flash, programmed the flash, then verified ok. Now the sn8200 is non-functional, I have tried re-flashing a number of times but it stays non-functional. Can somebody please give me some ideas on what I can try to get this module up and running. Note to Admin, if the community cannot help can someone from element14 talk to Embest for a way forward please.

 

Dave.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Just had a long hard look at the module J3 jtag connector on the module, looks like its not compliant! Embest have missed JTDI out, then followed on with JTMS in its place, so the rest of the pins including JTMS are 1 pin out! I will try and solve this with a cross over.

     

    Dave.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I cannot solve this with a crossover, if JTDI is missing, then its missing, but I can't be sure, programming the device passed even though the module is nonfunctional. Can Element14 please check document Discover Wi-Fi UserManual_V4.pdf table 2_1, to make sure the information is correct.

     

    EDIT: Table 2-1 is incorrect! Figure 2-3 schematic shows J3 and it's connections, I hope these are correct! See attached pdf.

     

    Dave.

    Attachments:
    imageDiscover Wi-Fi UserManual_V4.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Fixed! Please see here for the answer http://www.element14.com/community/thread/31278/l/embedded-group-or-not

     

    Dave.