Wireless
  • Technologies
  • More
Wireless
Forum wifi signal booster / antenna type
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 215 subscribers
  • Views 1446 views
  • Users 0 members are here
  • wifi
Related

wifi signal booster / antenna type

sivaguru
sivaguru over 3 years ago

Hello Everyone!!

I am so curious to know whether there are readily available Wi-FI signal booster for one of my project.

Idea & Use case is to enhance the signal strength from AP to STA with thick wall behind the AP and before STA. Would be great if anyone could point to any MUMIMO kind of antenna solution or a signal booster kind of product.

i am using wroom esp 32 development board (works only 2.4Ghz)

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +2
    Probably one reason no one is commenting, is because you seem to have made a conclusion that you need a new antenna or signal booster, when it's far from clear that this is the case. Engineers don't like…
  • robogary
    robogary over 3 years ago +1
    Sorry for the dumb question, why don't standard home wifi boosters work for you ?
Parents
  • shabaz
    0 shabaz over 3 years ago

    Probably one reason no one is commenting, is because you seem to have made a conclusion that you need a new antenna or signal booster, when it's far from clear that this is the case. Engineers don't like patching stuff on top of possibly incorrect initial conclusions by the (let's say) "client"!

    If the signal currently is so weak through a wall, then higher power (through signal booster or antenna) isn't likely to make as much of an improvement as one might think.

    There are legal issues too. If you've already configured the ESP32 to transmit at the most power that is supported, then you shouldn't boost the power.

    Some (better) options are to simply move the ESP32 (extend it with wires if you must, and deal with that hardware-wise in case the wire lengths cannot trivially be extended for signal integrity reasons), or move or add an access point closer to the ESP32.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 3 years ago

    Probably one reason no one is commenting, is because you seem to have made a conclusion that you need a new antenna or signal booster, when it's far from clear that this is the case. Engineers don't like patching stuff on top of possibly incorrect initial conclusions by the (let's say) "client"!

    If the signal currently is so weak through a wall, then higher power (through signal booster or antenna) isn't likely to make as much of an improvement as one might think.

    There are legal issues too. If you've already configured the ESP32 to transmit at the most power that is supported, then you shouldn't boost the power.

    Some (better) options are to simply move the ESP32 (extend it with wires if you must, and deal with that hardware-wise in case the wire lengths cannot trivially be extended for signal integrity reasons), or move or add an access point closer to the ESP32.