Wireless
  • Technologies
  • More
Wireless
Forum Omnidirectional RFID UHF antennas with medium (~25mm) range recommendations?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 215 subscribers
  • Views 4904 views
  • Users 0 members are here
  • antennas
  • rfid
Related

Omnidirectional RFID UHF antennas with medium (~25mm) range recommendations?

penguin
penguin over 2 years ago

Please bear with me as I couldn't even be considered a novice yet. I'm just a coder with an idea that I want to try out using RFID technology.


I want to identify and record data from passive RFID tags that are up to approximately 10 inches (25 cm) away from the device in any direction. There may be a few inches of low density foam between the antenna and the RFID tags. Small size and weight are important factors. Number of simultaneous tag reads... let's say, up to 5 at a time.

Based on my online research, I've come to the conclusion that a UHF reader is the way to go however, it seems like all antennas are either very short (few inches) or very long range. Can anyone recommend some antennas that might be suitable for these requirements?

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +3
    You didn't mention what region you require operation in, but if it's Europe, then this antenna looks ideal and is low-cost: https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000468/21442857 It…
  • shabaz
    shabaz over 2 years ago in reply to shabaz +3 suggested
    Board with the 868 MHz ceramic patch antenna attached. The underside has the U.FL connector, and should have a 0-ohm resistor, but I've not soldered that in yet (because I want to measure the impedance…
  • shabaz
    shabaz over 2 years ago in reply to shabaz +3 suggested
    Measurements! The results are not significantly different from the datasheet, for almost 2/3 of the frequency span. I wouldn't expect it to be identical anyway since there's no guarantee I tested in…
Parents
  • shabaz
    0 shabaz over 2 years ago

    That's quite normal, because a lot of antennas need some distance (far-field) to perform well. Whereas, in the range you're looking at (near-field), you're likely at the extremity of signal strength at 10 inches at UHF for near-field antennas. Compounding that, is that you're looking for a very wide radiation pattern which means signal strength will not be concentrated.

    I'm no expert, but I suspect you might need a far-field antenna positioned at a greater distance (I don't know your application). The far-field antenna at a distance will get you the coverage you desire without the need for a closer (near-field) antenna with omnidirectionalty I think. It's probably worth talking to either an antenna manufacturer or the RFID reader manufacturer (who will be quite experienced because they know what their customers use).

    Also, tag antenna shape/size will make a big difference, so you might want to experiment with several (assuming that's something you are able to modify in the solution).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago

    That's quite normal, because a lot of antennas need some distance (far-field) to perform well. Whereas, in the range you're looking at (near-field), you're likely at the extremity of signal strength at 10 inches at UHF for near-field antennas. Compounding that, is that you're looking for a very wide radiation pattern which means signal strength will not be concentrated.

    I'm no expert, but I suspect you might need a far-field antenna positioned at a greater distance (I don't know your application). The far-field antenna at a distance will get you the coverage you desire without the need for a closer (near-field) antenna with omnidirectionalty I think. It's probably worth talking to either an antenna manufacturer or the RFID reader manufacturer (who will be quite experienced because they know what their customers use).

    Also, tag antenna shape/size will make a big difference, so you might want to experiment with several (assuming that's something you are able to modify in the solution).