Wireless
  • Technologies
  • More
Wireless
Forum Omnidirectional RFID UHF antennas with medium (~25mm) range recommendations?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 215 subscribers
  • Views 4904 views
  • Users 0 members are here
  • antennas
  • rfid
Related

Omnidirectional RFID UHF antennas with medium (~25mm) range recommendations?

penguin
penguin over 2 years ago

Please bear with me as I couldn't even be considered a novice yet. I'm just a coder with an idea that I want to try out using RFID technology.


I want to identify and record data from passive RFID tags that are up to approximately 10 inches (25 cm) away from the device in any direction. There may be a few inches of low density foam between the antenna and the RFID tags. Small size and weight are important factors. Number of simultaneous tag reads... let's say, up to 5 at a time.

Based on my online research, I've come to the conclusion that a UHF reader is the way to go however, it seems like all antennas are either very short (few inches) or very long range. Can anyone recommend some antennas that might be suitable for these requirements?

Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +3
    You didn't mention what region you require operation in, but if it's Europe, then this antenna looks ideal and is low-cost: https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000468/21442857 It…
  • shabaz
    shabaz over 2 years ago in reply to shabaz +3 suggested
    Board with the 868 MHz ceramic patch antenna attached. The underside has the U.FL connector, and should have a 0-ohm resistor, but I've not soldered that in yet (because I want to measure the impedance…
  • shabaz
    shabaz over 2 years ago in reply to shabaz +3 suggested
    Measurements! The results are not significantly different from the datasheet, for almost 2/3 of the frequency span. I wouldn't expect it to be identical anyway since there's no guarantee I tested in…
Parents
  • shabaz
    0 shabaz over 2 years ago

    You didn't mention what region you require operation in, but if it's Europe, then this antenna looks ideal and is low-cost:

    https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000468/21442857 

    It is omni-directional, and I suspect (can't guarantee it, you'd need to try it) that it may support the range you're looking at.

    However, you'd need to mount it to a 70 x 70 mm ground plane, which is pretty easy to DIY (you can get the PCB ground plane manufactured for sub-$10, even in single quantity, from many PCB manufacturers in China).

    If you're in North America, then this antenna looks suitable:

    https://www.digikey.co.uk/en/products/detail/kyocera-avx/9000469/21442939

    Again, it requires the 70 x 70 mm ground plane. If you need more info about how to make the ground plane, let me know.

    (And again, no guarantee it will support the range you're looking for, but at the low price it's definitely worth a shot.

    The ground plane will end up looking something like this (the example here is for GPS, not RFID, but it will be almost identical).

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 2 years ago in reply to shabaz

    I ended up creating a PCB that will accept those antennas (or GPS antennas, and some other patch antennas too):

    image

    All it needs (other than the patch antenna) is a 0-ohm resistor (0805 or 0603 sized) and a U.FL socket (an example is Molex 73412-0110).

    There's space on the board for matching components if it comes to that, but it should be unnecessary.

    image

    The board fits some Hammond plastic enclosures (ideally, glue the board on the edges inside, to avoid using metal screws).

    Also an RF cable is needed (U.FL on one end, and whatever desired connector on the other).

    In case anyone wants such a generic patch antenna board, the zipped PCB files are here (ready for directly uploading to any PCB manufacturer). It costs £30 GBP to order 15 of these boards, with ENIG finish, including shipping. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 2 years ago in reply to shabaz

    I ended up creating a PCB that will accept those antennas (or GPS antennas, and some other patch antennas too):

    image

    All it needs (other than the patch antenna) is a 0-ohm resistor (0805 or 0603 sized) and a U.FL socket (an example is Molex 73412-0110).

    There's space on the board for matching components if it comes to that, but it should be unnecessary.

    image

    The board fits some Hammond plastic enclosures (ideally, glue the board on the edges inside, to avoid using metal screws).

    Also an RF cable is needed (U.FL on one end, and whatever desired connector on the other).

    In case anyone wants such a generic patch antenna board, the zipped PCB files are here (ready for directly uploading to any PCB manufacturer). It costs £30 GBP to order 15 of these boards, with ENIG finish, including shipping.