Wireless
  • Technologies
  • More
Wireless
Forum Do you have experience on connecting a Sub-1GHz transceiver to public TV antenna?
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 215 subscribers
  • Views 3819 views
  • Users 0 members are here
  • ISM band Sub-1GHz
Related

Do you have experience on connecting a Sub-1GHz transceiver to public TV antenna?

HKPhysicist
HKPhysicist over 1 year ago

Dear RF Engineers and Applied Physicists,

What are your experiences on connecting a Sub-1GHz transceiver to a public TV antenna?  Thinking

Since I live in a very dense city with skyscrapers, I cannot set up my own antenna outside my building.  Then, I want to wire my own SMA Male to TV Male Plug coaxial cable.  This will connect my Sub-1GHz transmitter directly to my building`s public TV antenna.

The next step is to connect my ISM band Sub-1GHz transmitter to test a receiver several hundred metres to 1km away.

Who have experience on this?  What else should I do to improve the transmission or communication?  I guess a high quality Element14 MultiComp coaxial cable can serve well.  Satellite

Thanks for your opinions.  Nerd

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 1 year ago in reply to HKPhysicist +2
    "I will use my building's public antenna." "I have never seen our public antenna. We cannot access our roof." I don't think you understand; if you still mean the TV antenna, it's not a public "anyone…
  • JWx
    JWx over 1 year ago +1
    In my country many TV antennas are advertised as including LTE filters (probably strong cellular signal is disrupting TV signal). Other points to consider: building's public antenna installation can…
  • shabaz
    shabaz over 1 year ago +1
    It might be good to take a step back. It could be worth mocking up something, like a quick tryout, to see what issues there could be, if you're new to this. For example, you might find that the performance…
Parents
  • shabaz
    shabaz over 1 year ago

    It might be good to take a step back. It could be worth mocking up something, like a quick tryout, to see what issues there could be, if you're new to this.

    For example, you might find that the performance from a modem, is already as good as it is for your mobile phone. Maybe any bottlenecks are less to do with the antenna.

    Once you've gathered some information, then it's best to spend time to design the overall solution first, before getting into this.

    What if your solution needs two modems, will you attach a second TV antenna? On second pole on the building? As you can see, just that slight requirement (sure it's hypothetical, I'm using it as an example) would then render the idea impractical now regardless of the technical concerns of your antenna and cable (of which there are for sure concerns; none of that will be ideal unfortunately). By the way, you can buy antennas (either indoor or outdoor) designed for cellular use.

    If you're designing all this from scratch, then if it were me, I'd try if possible, as part of the overall design, to locate such things at a suitable position and then run low-cost cable (e.g. cat5, it's less than $1 per meter) all the way to where you want to locate anything else (if you're not say using wireless; I have no idea what your solution is going to look like). There may be reasons not to do that, but it would at least be worth considering (if you have not already ruled it out), since there's a chance it would be more practical. But definitely worth a quick experiment first I think; because I think you're unsure what will work at all, if you're currently considering TV antennas.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • HKPhysicist
    HKPhysicist over 1 year ago in reply to shabaz

    Thanks for your valuable opinion.

    I have solved the LTE CAT M1 modem problem by simply orienting its location around my home.  Signal strength reported by my laptop Network Manager is about 85%.

    My next test is to set up an ISM band Sub-1GHz antenna to connect to my Sub 1GHz transceiver which will then talk with my receiver half to one km away.

    This is my first field RF project, very exciting!  Blush

    I will use my building's public antenna.  As my target is civil ISM band under 20dbm radio power, I do not violate any radio rule.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to HKPhysicist
    This reply was deleted.
    • Cancel
    • Cancel
  • HKPhysicist
    HKPhysicist over 1 year ago in reply to anniel747

    My new antenna is 10-12dbi, 9in tall and 3in in diameter, a huge antenna.

    I have never seen our public antenna.  We cannot access our roof.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • HKPhysicist
    HKPhysicist over 1 year ago in reply to anniel747

    So I have to use 50 Ohm coaxial cable, right?  They are quite expensive - 2 pounds per meter.

    https://hk.element14.com/huber-suhner/enviroflex-b58/coaxial-cable-rg58-50-ohm-per/dp/2817372

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • HKPhysicist
    HKPhysicist over 1 year ago in reply to anniel747

    So I have to use 50 Ohm coaxial cable, right?  They are quite expensive - 2 pounds per meter.

    https://hk.element14.com/huber-suhner/enviroflex-b58/coaxial-cable-rg58-50-ohm-per/dp/2817372

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • anniel747
    anniel747 over 1 year ago in reply to HKPhysicist
    This reply was deleted.
    • Cancel
    • Cancel
  • HKPhysicist
    HKPhysicist over 1 year ago in reply to anniel747

    Ok, thanks for your opinions.

    I am going to shop an antenna impedance tuner or solder one for my self.

    I've found this post very informative.

    www.ad5gg.com/.../