Wireless
  • Technologies
  • More
Wireless
Forum RF ESD protection
  • Blog
  • Forum
  • Documents
  • Polls
  • Quiz
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Wireless to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 221 subscribers
  • Views 4271 views
  • Users 0 members are here
Related

RF ESD protection

nicoloquinte
nicoloquinte over 8 years ago

Hi,

I'm entering the beautiful world of RF design, and after looking into the documentation of the ublox NEO-6M module and saw this:


image

 

So because i know that my antenna is absolutely perfect (that isn't true but i'm proud of my qfh garbage)

I need to go with the inductance method since some manufacturers are saying that I should not go with a TVS because that's doing Bad things to the signal :

https://www.murata.com/products/emc/esd/sol_antenna_noise

 

So Do someone have any idea about how I can calculate the inductance

 

(BTW i wont connect my antenna directly to the RF-IN like this , i will do a little step of filtering)

 

Nico

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago in reply to shabaz +3
    Usually you add an inductor to try and make the final stage think the antenna is matched, when in fact it isn't. Any mismatched antenna will not radiate 100%, so it's best to avoid them if you have low…
  • shabaz
    shabaz over 8 years ago in reply to mcb1 +3
    We did the same too : ) and test with a short burst, it was very cool hearing the relays clicking away, doing their ATU selection : ) I didn't look closely at what the module was, but guessed it was a…
  • shabaz
    shabaz over 8 years ago in reply to nicoloquinte +2
    Hi Nicolas, The part will be tiny (of the order of 1mm in dimensions) because of the capacitance mentioned earlier, that needs to be minimized, otherwise there will be no usable signal. 1mm is hand-solderable…
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Nico,

     

    You can calculate the impedance and just ensure it is significantly higher than 50 ohms, for the frequency that you're working at. However, the real-world inductor will also have capacitance. At the frequencies that device will operate at, you can't use any inductor. I think option 3 in the document will be easier. Also, there is further reasoning to support this and suggestions for option 3 here:

    https://www.murata.com/en-eu/products/emc/esd/sol_antenna_loss

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to shabaz

    Usually you add an inductor to try and make the final stage think the antenna is matched, when in fact it isn't.

    Any mismatched antenna will not radiate 100%, so it's best to avoid them if you have low power or have very little spare path loss.

     

    We have them as auto tune units on HF aerials to compensate for droop, and bird loading ..

    They work well until 2-300 hundred starlings decide its a great perch, and it can't compensate.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    We did the same too : ) and test with a short burst, it was very cool hearing the relays clicking away, doing their ATU selection : )

    I didn't look closely at what the module was, but guessed it was a GPS module, in which case even the metre of co-ax is significant from the passive antenna. It is nice that electronics nowadays is so tiny, it is possible to put the entire radio (or major chunks of it) right at the antenna, rather than trail coax down to a receiver.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago in reply to mcb1

    We did the same too : ) and test with a short burst, it was very cool hearing the relays clicking away, doing their ATU selection : )

    I didn't look closely at what the module was, but guessed it was a GPS module, in which case even the metre of co-ax is significant from the passive antenna. It is nice that electronics nowadays is so tiny, it is possible to put the entire radio (or major chunks of it) right at the antenna, rather than trail coax down to a receiver.

    • Cancel
    • Vote Up +3 Vote Down