3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Brittle PLA
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 25 replies
  • Answers 17 answers
  • Subscribers 338 subscribers
  • Views 5206 views
  • Users 0 members are here
  • pla
  • white_pla
  • 3D Printing
  • robox
  • cel_robox
Related

Brittle PLA

danielw
danielw over 9 years ago

Has anybody had any issues with PLA going brittle?  At work we have a CEL Robox and I've noticed that some white PLA filament that was on the end of a spool and lying around for several months has gone brittle and snaps easily. New filament is much more bendy.

 

We have a windowless office so it has only seen fluorescent light, so I guess that it's to do with moisture in the air.  We keep current filament in ziplock bags with silica gel packs.

 

I know that PLA is supposed to be bio degradable so maybe it's just degrading?  I'm wondering if the same will happen to finished parts?  I'm planning to print out some test strips and test them over time, but wondered if anybody has any good info on this and point to a good online resource.  I'll also be having a look on the CEL site for info.

 

I suppose this is possibly another reason for using ABS on my REP RAP bodge-o-matic printer at home!  I thought I'd get away with PLA if it wasn't too hot.

 

Dan.

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 9 years ago +5 suggested
    Hello Daniel, The problem is not specifically related to PLA, but - in a different measure - it occurs also with ABS. Anyway PLA filament is subject to degrading almost easily than ABS. This is the reason…
  • gregoryfenton
    gregoryfenton over 9 years ago +5 suggested
    I regularly change the colours of the materials I use meaning that I have lots of partly used rolls. The simple technique I use is to put each roll in a bag, pierce a small hole for the filament to pull…
  • dougw
    dougw over 9 years ago +4 suggested
    My experience is that the tendency to become brittle is much more likely in the section of PLA that is in the printer, perhaps because of exposure to heat. Maybe the pigment material starts annealing into…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Interesting topic. I don't know if this is useful, but there's a long article here:

    https://onlinelibrary.wiley.com/doi/full/10.1111/j.1541-4337.2010.00126.x

    some snippets like this seemed interesting to me, but probably worth reading in full:

    image

     

    One problem is that most information out there concerns PLA for non-3D-printing applications, like food packaging, or medical use inside humans since it biodegrades safely.

    So for example, the above snippet refers to PLA sheet, but I don't know if bendy PLA filament is acceptable to consider as a sheet.. I think it is, but it's a guess for me.

    I don't have any hard conclusions (and I don't own a 3D printer or PLA so I have no personal experience, but it's still an interesting topic for me to learn more from others) but from some of the research from non-3D-print applications, it seems that for PLA, moisture, or moisture and heat together, can cause some irreversible effects, and some reversible effects. Some things can be controlled, but realistically many people are working in environments that easily approach or exceed 50% RH, and cooling is to room temperature fairly quickly unlike a controlled environment like an oven.

     

    It's very cool that people have found out some mitigation like removing unused filament and wrapping it up, or cutting off the heated end, etc. Even if the precise underlying physics isn't know, that experience is valuable. For example, when I cut acrylic, I can see that the melted acrylic is more brittle, but I don't know the physics to it. I just know I really need to avoid it getting toward melting stage, otherwise I can't machine that area further (apparently additives can reduce brittleness with such heat scenarios with some plastics, according to https://www.bpf.co.uk/plastipedia/additives/default.aspx  - anyway it's a digression). Also maybe if PLA in filament form is really just considered as a consumer hobby material by some manufacturers, there could be less controls, or alternatively might have their own mixes with additives to help with the brittleness? Just speculation : (

    Also, as an idea, maybe design-level things can be done to mitigate too, e.g. have 3D printed shapes with thicker regions to change cooling rate (if that is an issue) or curves in multiple planes, to minimize flex of the completed item during use, i.e. perhaps design the item slightly differently if using a specific plastic.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Interesting topic. I don't know if this is useful, but there's a long article here:

    https://onlinelibrary.wiley.com/doi/full/10.1111/j.1541-4337.2010.00126.x

    some snippets like this seemed interesting to me, but probably worth reading in full:

    image

     

    One problem is that most information out there concerns PLA for non-3D-printing applications, like food packaging, or medical use inside humans since it biodegrades safely.

    So for example, the above snippet refers to PLA sheet, but I don't know if bendy PLA filament is acceptable to consider as a sheet.. I think it is, but it's a guess for me.

    I don't have any hard conclusions (and I don't own a 3D printer or PLA so I have no personal experience, but it's still an interesting topic for me to learn more from others) but from some of the research from non-3D-print applications, it seems that for PLA, moisture, or moisture and heat together, can cause some irreversible effects, and some reversible effects. Some things can be controlled, but realistically many people are working in environments that easily approach or exceed 50% RH, and cooling is to room temperature fairly quickly unlike a controlled environment like an oven.

     

    It's very cool that people have found out some mitigation like removing unused filament and wrapping it up, or cutting off the heated end, etc. Even if the precise underlying physics isn't know, that experience is valuable. For example, when I cut acrylic, I can see that the melted acrylic is more brittle, but I don't know the physics to it. I just know I really need to avoid it getting toward melting stage, otherwise I can't machine that area further (apparently additives can reduce brittleness with such heat scenarios with some plastics, according to https://www.bpf.co.uk/plastipedia/additives/default.aspx  - anyway it's a digression). Also maybe if PLA in filament form is really just considered as a consumer hobby material by some manufacturers, there could be less controls, or alternatively might have their own mixes with additives to help with the brittleness? Just speculation : (

    Also, as an idea, maybe design-level things can be done to mitigate too, e.g. have 3D printed shapes with thicker regions to change cooling rate (if that is an issue) or curves in multiple planes, to minimize flex of the completed item during use, i.e. perhaps design the item slightly differently if using a specific plastic.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer