Arduino Forum MQTT client program not showing any results with Arduino
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
  • Replies 49 replies
  • Subscribers 405 subscribers
  • Views 4596 views
  • Users 0 members are here
Related

MQTT client program not showing any results with Arduino

Former Member
Former Member over 10 years ago

I modified the MQTT example present under MQTT library pubsubclient for Arduino.

My MQTT server address is 192.168.1.6 with port 8081.

To this MQTT server,another MQTT client in my mobile is able to connect.

But this is not working with Arduino.There is no error shown during compilation or during uploading.

Infact,I am not able to see the connection result messages such as "Connected" or "Not connected" which i given in Serial.println() in setup function.

I am resetting Arduino before uploading the program.Please let me know why this is not showing any output....

 

#include <SPI.h>

#include <Ethernet.h>

#include <PubSubClient.h>

// Update these with values suitable for your network.

byte mac[]    = {  0xDE, 0xED, 0xBA, 0xFE, 0xFE, 0xED };

byte server[] = {192, 168, 1, 6 };

//byte ip[]     = { 172, 16, 0, 100 };

 

 

void callback(char* topic, byte* payload, unsigned int length) {

  // handle message arrived

}

EthernetClient ethClient;

PubSubClient client(server, 8081, callback, ethClient);

void setup()

{

  Ethernet.begin(mac);

  if (client.connect("*")) {

     Serial.begin(9600);

    Serial.println("Connected to MQTT Server");

    client.publish("outTopic","hello world");

   // client.subscribe("inTopic");

  }

  else

  {

   Serial.println("Could not connect to MQTT Server");

  }

}

void loop()

{

  //client.loop();

 

}

  • Sign in to reply
  • Cancel

Top Replies

  • neilk
    neilk over 10 years ago in reply to Former Member +3
    generk4 and organtin Hi Radhamani and Giovanni - I had 30 minutes to spare so I copied the program from comment 19 and posted it into the Arduino IDE (I am using 1.6.1), compiled and uploaded it to a genuine…
  • Former Member
    Former Member over 10 years ago +3
    Hi Bob, Neil and Clem, I tried LM35 Temperature sensor with MQTT Arduino sketch and it works fine for me I am sooo happy Thanks once again for your wonderful support and help
  • Former Member
    Former Member over 10 years ago in reply to bobcroft +2
    Hi bob,Neil,Clem and many others who have helped and guided me in this issue, I have successfully completed MQTT program and Arduino is successfully publishing and subscribing messages Next step,I am going…
Parents
  • Former Member
    Former Member over 10 years ago

    Hi Bob,Neil and Clem,

       I tried LM35 Temperature sensor with MQTT Arduino sketch and it works fine for me image

    I am sooo happy image Thanks once again for your wonderful support and help image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to Former Member

    generk4  Hi Radhaman That really is excellent news. I hope you can complete your project now. Please let us know. image

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neilk
    neilk over 10 years ago in reply to Former Member

    generk4  Hi Radhaman That really is excellent news. I hope you can complete your project now. Please let us know. image

     

    Neil

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 10 years ago in reply to neilk

    Hi all...

    I have completed my project successfully image Thanks again for your wonderful support imageThis forum is rocking !!!!

     

    Lessons learnt :-

      1) We have to press the Ethernet shield very tightly with Arduino board

      2) If basic DHCP program does not work even after tight connection of Ethernet shield and Arduino board,we need to check with the vendor whether its fault on the component.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Former Member

    DHCP does work with the standard Ethernet shield, I have used it on many occasions

     

    You may want to also check you DHCP server ?

     

    regards

     

    Peter