Circuit Protection
  • Technologies
  • More
Circuit Protection
Forum Why is this transistor required
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Circuit Protection to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 71 subscribers
  • Views 2197 views
  • Users 0 members are here
  • relay
Related

Why is this transistor required

rishi2628
rishi2628 over 9 years ago

Why is the transistor Q3 required in this circuit of a optocoupler and a relay. Can't I directly attach the power pin of the relay to the opto coupler pin 3 and ground the other pin of the relay. I tried it and it works. Just want to know why is it not implemented and why is the transistor required.

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • spannerspencer
    spannerspencer over 9 years ago in reply to rishi2628 +1
    Ah yes, I see what you mean. Possibly the switching current for the relay coil is higher than the optocoupler can safely provide, so the transistor is there to do the job instead.
Parents
  • rishi2628
    0 rishi2628 over 9 years ago

    If you cannot view the image then try this link:-

    https://drive.google.com/file/d/0B2HbfYZlVykfcWJ5TUpDNFh1Z0k/view

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rishi2628
    0 rishi2628 over 9 years ago

    If you cannot view the image then try this link:-

    https://drive.google.com/file/d/0B2HbfYZlVykfcWJ5TUpDNFh1Z0k/view

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to rishi2628

    You don't provide enough information for a definitive answer - for which I would need the part numbers or specs of the relay and the opto-coupler.

     

    However, typically a normal opto-coupler will have a coupling of between 10% and 50% - which means that for 5mA in the LED you can expect a collector current of between 0.5 and 2.5mA maximum. The relay will probably need a current of about 50mA to turn on.

    Some opto-couplers are specified for much higher gains so may be able to reliably operate the relay but it is likely that using a standard low cost opto-coupler and  a transistor will be cheaper and offer a greater operating margin.

     

    Another thing to look out for in the coupler spec is the maximum output current - which may not be enough to operate the relay.

     

    For future reference, when you ask a question on a forum like this the quality of the answer will depend on the information you provide - please try to include part numbers for all the key components.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rishi2628
    0 rishi2628 over 9 years ago in reply to michaelkellett

    These are the datasheet values for the opto coupler. Hope it helps:-

     

    Collector-base voltage . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 70 V

    Collector-emitter voltage (see Note 1) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 30 V

    Emitter-collector voltage . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 V

    Emitter-base voltage . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7 V

    Input-diode reverse voltage . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3 V

    Input-diode continuous forward current . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 60 mA

    Input-diode peak forward current (tw ≤ 1 ns, PRF ≤ 300 Hz) . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3 A

     

     

    Could the transistor be in the circuit just to save the opto coupler ic. I mean if due to some reason the opto coupler gets damaged, it would be more expensive to replace the ic but if we just use a transistor that gets destroyed, we need to pay less money to fix it....What do you think??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to rishi2628

    You haven't given me the key opto-coupler parameter - what's the coupling coefficient (current transfer ratio) ?

     

    Take a look at the data sheet for Farnell 2323137 a Farichild  FOD817FOD817 on page 4 they give the key parameters in the table"DC Transfer Characteristics there will be a similar table in the data sheet for the device you have

     

    MK