Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog BT_Sentry : Sentry Power
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
  • Author Author: mcb1
  • Date Created: 26 May 2018 8:24 AM Date Created
  • Views 2684 views
  • Likes 12 likes
  • Comments 8 comments
  • bluetooth
  • solar-cell
  • raspberry pi 3 b+
  • rf signal
  • pi camera
  • cypress
  • solar
  • bt_sentry
Related
Recommended

BT_Sentry : Sentry Power

mcb1
mcb1
26 May 2018

This is the 4th of my Blogs for the Bluetooth Unleashed Design Challenge

 

 

The other posts are here :-

Link to other posts
BT_Sentry Introduction
BT_Sentry : Zero Emission Detection
BT_Sentry : Data Transmission

 

Concept

The idea is to detect the bluetooth transmitted from the vehicle and signal other Home Automation functions.

If the vehicle is known then it can open the garage door, and inform the home owner that xx is home.

 

Hardware

The detection point needs to be at the start of the driveway, and because there is no power source, this will need to be low power with solar charging.

The PSOC range seems a very good fit, but because of the timeline and my need to upskill, the inital design will be Arduino based and some form of RF transmitter/transceiver.

 

Adding a vehicle detection loop or beam is necessary to ensure those vehicles without bluetooth will also trigger the system.

 

 

 

By now I'd hoped to be blogging about Bluetooth detection, but it hasn't been progressing very fast ... in fact I haven't had it running at all.

That isn't to say I haven't been doing some research, understanding and a few examples.

 

 

 

 

Solar Power

Because the gateway (Sentry) location is unpowered, I'm going to require solar (or wind) to charge the battery.

 

While it might be ideal to use the BLE characteristics, the reality is that I need to advertise, and that takes energy.

Most of the BLE (Bluetooth Low Energy) devices are the receiving end, so they simply wait until they wake up and detect someone advertising, and then connect and communicate.

 

Obviously most 'visitors' that I'm interested in, aren't going to connect, or be connected previously, and since I don't intend providing any services, its will just be a MAC address gathering exercise.

 

Ideally I'd like to know just how much power I need, but the reality is I don't, so I thought I'd look at some possible options.

 

 

 

 

 

Solar Lights

I recently visited a friends place where he runs off solar power.

The cost of getting the power even to his gate, is prohibitive, and his permanent house is still being planned (and financed).

 

He was using some low cost solar lights that one of the local retailers had, and they worked very well.

 

When I was visiting another retailer, I spotted these, and the importance was they used a 3.2v battery, rather than the single cell many others have.

The costs was NZ$15, and if they weren't suitable, I could still use them as they were designed.

 

imageimage

 

 

Strangely they must be designed for another use, as the mounting bracket seems to also fit the solar panel ....

You can see there is room inside for some electronics, so it could be very useful even as a solar powered PIR detector.

imageimageimage

As the pictures show, the construction is simple, with plenty of hot glue to hold the board and lens in place, while a bit of foam supports the 3.2v 400mAH battery.

 

 

 

Shed Light

While I was picking up 2 more of the above, I looked at a Shed light.

The idea is you have a solar panel outside, and a LED light inside where it would otherwise be dark.

 

The LED is just a few LEDs in parallel with a small resistor, so not exactly efficient, but I wasn't after it for the Light .... just the panel.

The box suggested it used 3 rechargable cells, which by my calculation is 3.6 volts.

 

Once opened it reveals three standard rechargable cells 1.2v 200mAH.

So not as high as the other lights, but I'll need to do some tests to see what the panel can deliver before seeing if it is useful.

 

imageimage

The last photo shows the build quality you can expect with these cheap devices.

The battery clip on both sides has been installed upside down, while the soldering has been while the battery is installed.

 

I do like the pull switch. It's a rather clever way to achieve it.

 

Unlike the other lights, this is definately not an outdoor unit.

BUT having seen the poor design of other 'outdoor' units, I tend to treat them all with some scepticism nowdays image

 

 

 

 

 

Parts

My shopping basket is on it's way thanks to the generousity of element14/Newark and the work by danzima and UPS.

I'm not sure if that arrives before I go, but it isn't a requirement just yet.

 

After a discussion between Jan Cumps and myself regarding the current consumption

https://www.element14.com/community/community/design-challenges/bluetoothunleashed/blog/2018/04/30/btsentry-introduction…

I purchased a Cypress Low Energy BLE kitCypress Low Energy BLE kit  and I've ordered a solar powered version Cypress Solar BLE

 

Sadly there are none available on the NZ website and e14phil kindly checked his cupboard, but alas there were none lurking, so it is coming directly from Cypress

 

 

It could be that after all this, I just use the CY8C4248LQI-BL583 module on its own as the size is right and it seems that the MCU is onboard.

Whatever the outcome, fvan is safe from blame for buying these ....image

 

 

 

 

Next Blog

I'm away on holiday next week, so I'm going to see if I can prepare the next blog, and try the scheduled posting.

Unless you'd all prefer photos of cars and a warm beach with people swimming ...image

 

 

Mark

  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice update Mark. DAB
  • shabaz
    shabaz over 8 years ago +2
    Hi Mark! It's a really cool idea to have your project solar powered. Also, interesting teardown to see what is inside these existing solar powered products! I hope you have an excellent time off at the…
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel +2
    How did you know they had the 3.2v battery in them? It was a tricky prospect for us Engineering types ... The shed Light was also a struggle (especially if you leave your glasses in the car) I did have…
  • genebren
    genebren over 8 years ago in reply to mcb1

    Mark,

    Very interesting article on battery and solar panel sizing.  Solar power is one of those things that look simple on the outside, but get incredibly complex on the inside.  I worked on larger residential and commercial charger/inverter designs many years ago, which was a challenge, but also a lot of fun.  Between safe charging practices, peak power tracking (ideal voltage/current relationships) and sizing (as you mentioned above), not to mention regulatory requirements, there becomes a lot of variables to consider. You are correct too, about the need for buck/boost converters required to keep all of the voltages in the optimal range for the proper system functioning.

     

    Funny how a Bluetooth challenge, becomes a challenge in so many other aspects of system design.

    Good Luck!

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    Wow, that's amazingly clear - I've seen less information on rechargeable battery packs here, like they obfuscate the details on purpose!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel

    How did you know they had the 3.2v battery in them?

    It was a tricky prospect for us Engineering types ...

    image

     

    The shed Light was also a struggle (especially if you leave your glasses in the car)

    image

     

     

     

    I did have the ES8266 sensor in mind for these.

    I have a couple of other projects and it seemed ideal.

     

    The Warehouse is also quite good at stocking replacement batteries at very reasonable prices, so I'll have to see if they become available.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago

    Those 3.2v solar lights look like a great find!

    I've been thinking of using a 3.2v battery to power an ESP8266 based sensor, as the voltage range seems to fit well for the ESP voltage requirement without needing extra hardware.

     

    >I spotted these, and the importance was they used a 3.2v battery

    How did you know they had the 3.2v battery in them?

     

    Also, have you figured out a solution to avoid low voltage situations? Or do you just let it run til the power runs out?

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago

    genebren

    My earlier post  BT_Sentry Introduction  had some info in the discussions for anyone contemplating reliable Solar.

    https://nicegear.nz/blog/what-size-solar-panel-and-battery-do-i-need/

     

    I believe many of the later regulation systems use a buck/boost converter to convert the incoming energy into a suitable voltage.

    Previously the method was simply to regulate it so the batteries aren't cooked.

     

    This means that the solar panel is effectively more efficient with the sunlight available.

     

    The biggest issue with using larger batteries is that at some point to need to " pay the piper " ... that is, you need to recharge the battery.

    I've suggested to my friend that he split his batteries and charge one set, while using the other, otherwise he runs the risk of damaging them with the limited solar energy he has.

     

    I don't have that option, so I may need to go to a bigger panel.

     

     

    Thanks to everyone else for the comments.

    As I understand the radiation is so much that liquid cooling is the solution ....

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>