Bluetooth Unleashed Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Bluetooth Unleashed Design Challenge
  • More
  • Cancel
Bluetooth Unleashed Design Challenge
Blog Stirling Blue - Fuel Measurement - Blog 4
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
  • Author Author: dougw
  • Date Created: 21 May 2018 4:27 AM Date Created
  • Views 2485 views
  • Likes 17 likes
  • Comments 6 comments
  • stirling blue
  • doug wong
  • fuel measurement
  • bluetooth unleashed
  • bluetooth unleashed design challenge
Related
Recommended

Stirling Blue - Fuel Measurement - Blog 4

dougw
dougw
21 May 2018

The Stirling Blue project will be measuring several Stirling engine parameters including inputs and outputs so I can calculate efficiency. The input to the engine is fuel - alcohol in this case, and I will need to know how much is consumed. I could do a before and after weight measurement, but I want the PSoC6 to be able to monitor all parameters in real time. The gas tank is actually a 10 ml glass jar. The fuel is drawn out using a wick that also acts as the burner. This blog explores using capacitance to measure fuel level in the jar. I did an earlier road test of the TI FDC2214, which is a very accurate capacitance measurement circuit. This will be a good choice for measuring such a small jar. It uses an I2C interface so I will have to figure out how to get the PSoC6 talking to it.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Capacitance sensing of the fuel level with the FDC2214 works well. I may double the width of copper tape on the bottle to increase the capacitance values.

 

Upcoming blogs:

Blog 5 will be about how Stirling engines work

Blog 6 will start connecting some sensors to the PSoC6

Blog 7 will be about designing the sensor interface PCB

 

Related Links:

Bluetooth Unleashed Design Challenge

Bluetooth Unleashed Design Challenge: The Challengers

Bluetooth Unleashed Design Challenge: About This Challenge

 

Links to other blogs for this project:

Stirling Blue - Project Description - Blog 1

Stirling Blue - Unboxing Hero - Blog 2

StirlingBlue1

Stirling Blue - micro:bit TXTR - Blog 3

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +4
    Good work. Be interesting to see the rate of change with different vessels. The fact it's linear is a good start. Mark
  • dougw
    dougw over 8 years ago in reply to genebren +4
    It should burn at a pretty steady state rate so I can take some time to get a more precise measurement of level change.
  • genebren
    genebren over 8 years ago +3
    Doug, Great update on your project. The results do look promising. I am not sure how much fuel would normally be consumed during the running of your engine, but the rate of change on a few picofarads might…
Parents
  • genebren
    genebren over 8 years ago

    Doug,

    Great update on your project.  The results do look promising.  I am not sure how much fuel would normally be consumed during the running of your engine, but the rate of change on a few picofarads might be difficult to determine (or maybe not).

    Good luck!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Doug,

    Great update on your project.  The results do look promising.  I am not sure how much fuel would normally be consumed during the running of your engine, but the rate of change on a few picofarads might be difficult to determine (or maybe not).

    Good luck!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to genebren

    It should burn at a pretty steady state rate so I can take some time to get a more precise measurement of level change.

    • Cancel
    • Vote Up +4 Vote Down