Connected Cloud Challenge
  • Challenges & Projects
  • Design Challenges
  • Connected Cloud Challenge
  • More
  • Cancel
Connected Cloud Challenge
Blog The Bio Highway – Finishing the First Mile
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
  • Author Author: vlasov01
  • Date Created: 5 Apr 2020 1:47 AM Date Created
  • Views 695 views
  • Likes 3 likes
  • Comments 2 comments
  • amazon freertos
  • troubleshooting
  • modustoolbox
  • xming
  • mbed
  • afr
  • aws iot
Related
Recommended

The Bio Highway – Finishing the First Mile

vlasov01
vlasov01
5 Apr 2020

Which platform should I use - Amazon FreeRTOS or Mbed OS?

 

It is a good question to think about before investing a lot of time into a new platform as at the end our time is our most precious resource, It requires some analysis. I've googled Internet, but was not able to answer a good answer.

I've used Mbed OS two years ago on another IoT on Wheels Design Challenge  (you can read my blogs on Mbed OS IOT on Wheels Design Challenge - Smart Drive - First Steps with mbed os - Blog #2, IOT on Wheels Design Challenge - Smart Drive - MBed To The Rescue - Blog #7 , IOT on Wheels Design Challenge - Smart Drive - MBed with GPS Receiver - Blog #8 ). It is a fast growing web based collaborative platform. I believe it has all capabilities you are listed. And it was very light on PC hardware requirements. It was very easy to start development, build, deploy. There was almost no software to install/maintain on my machine.

But Amazon FreeRTOS (AFR) has additional capabilities, that seems important for some use cases - device onboarding, OTA updates, device shadow, secure storage, key management. Take a look at 10 minutes video IoT Edge Computing: Introduction to Amazon FreeRTOS I'm still looking forward to discover which of these extra capabilities of AFR are already supported on Cypress PSoC 6.

 

My plan for this challenge is to start with AFR/ModbusToolbox and keep Mbed OS as plan B, in case if run into dead end with plan A.

 

Here is the summary as I understand it after following AFR trainings, but before starting using it. I'll revise it as my understanding of it evolves.

Mbed OSAmazon FreeRTOS
Support of PSoC6 featuresyesyes
Support external peripheralsyesyes
AWS IoT connectivityyesyes
OTA updatesnoyes
Device on-boardingnoyes
Device shadownoyes
Secure storagenoyes
Key managementnoyes
Communityyesyes
Supportyesyes
Web-based building tool chainyesno
Web-based collaborative platformyesno

 

Why ModbusToolbox?

It is the recommended tool for AFR Cypress PSoC  development at this point.

 

Installing ModbusToolbox

I've followed ModusToolbox Installation Guide, but I've missed an important system requirement. It doesn't support the OS I'm using - Windows 10 32-bit. So I've got the error:

image

I have an old box with Ubuntu 18.04. It has only 1.5GB of RAM and one CPU core. It is much smaller than recommended for ModusToolbox.But installation completed successfully. And I was able launch it.

 

Screen Capture

The only problem so far - it is not convenient for me to snap pictures for this blog on Ubuntu.

I've attempted to solve it by using a remote display. I've installed xming X-Server on my Windows PC and than launched ModusToolbox on Ubuntu box.

cd ModusToolbox/ide_2.0/eclipse/
export DISPLAY=192.168.1.37:0.0
./ModusToolbox

Initially it was looking very promising, but than after I've started using it I've realized that some interfaces of the IDE where missing or distorted on my X-Server.

 

Firmware Loader upgrade

I've downloaded and installed the newer version of Cypress firmware loader fw-loader-2.3.0.568-linux to replace one that was provided with ModusToolbox.

 

Demo project

I've loaded demo project, build it and loaded to the board. No problem so far.

 

I've installed terminal emulator, so I can get output from the board:

sudo apt install screen

 

Than I've started the terminal emulator.

screen /dev/ttyACM0 115200

 

And I've started the demo program on the board:

0WLAN MAC Address : 00:9D:6B:63:76:09
WLAN Firmware    : wl0: Sep  5 2019 23:24:33 version 7.45.98.92 (r722362 CY) FWID 01-f7128517
WLAN CLM         : API: 12.2 Data: 9.10.39 Compiler: 1.29.4 ClmImport: 1.36.3 Creation: 2019-09-05 23:10:00
WHD VERSION      : v1.70.0 : v1.70.0 : GCC 7.2 : 2019-12-02 04:14:53 -0600
.1 5585 [Tmr Svc] Wi-Fi Connected to AP. Creating tasks which use network...
2 5585 [Tmr Svc] IP Address acquired 192.168.1.71
3 7301 [Tmr Svc] Write certificate...
4 7841 [iot_threa] [INFO ][DEMO][lu] ---------STARTING DEMO---------

5 7843 [iot_threa] [INFO ][INIT][lu] SDK successfully initialized.
.6 12654 [iot_threa] [INFO ][DEMO][lu] Successfully initialized the demo. Network type for the demo:7 12654 [iot_threa] [INFO ][MQTT][lu] MQTT library successfully initialized.
8 12654 [iot_threa] [INFO ][DEMO][lu] MQTT demo client identifier is bio01 (length 5).
.9 16322 [iot_threa] [INFO ][MQTT][lu] Establishing new MQTT connection.
10 16324 [iot_threa] [INFO ][MQTT][lu] Anonymous metrics (SDK language, SDK version) will be provid11 16325 [iot_threa] [INFO ][MQTT][lu] (MQTT connection 0x8012778, CONNECT operation 0x800c168) Wai.12 21325 [iot_threa] [INFO ][MQTT][lu] (MQTT connection 0x8012778, CONNECT operation 0x800c168) Wai13 21325 [iot_threa] [ERROR][MQTT][lu] Failed to establish new MQTT connection, error TIMEOUT.
14 21326 [iot_threa] [INFO ][MQTT][lu] Network connection closed on error.
15 21626 [iot_threa] [INFO ][MQTT][lu] (MQTT connection 0x8012778) Network connection destroyed.
16 21626 [iot_threa] [ERROR][DEMO][lu] MQTT CONNECT returned error TIMEOUT.
17 21626 [iot_threa] [INFO ][MQTT][lu] MQTT library cleanup done.
18 21626 [iot_threa] [ERROR][DEMO][lu] Error running demo.
19 21626 [iot_threa] [INFO ][INIT][lu] SDK cleanup done.
20 21626 [iot_threa] [INFO ][DEMO][lu] -------DEMO FINISHED-------

 

The board was able to connect to my WiFi network,but than it failed to connect with AWS IoT MQTT broker (line 14).

 

Unfortunately I was not able to find any debug information on the failed connection on AWS IoT Console.

 

I've opened support ticket at AWS IoT community forumhttps://community.cypress.com/message/229183#229183and at Cypress Community forum,

 

I was able to find the issue next day. It appeared that I missed one step in the on-boarding of the device and haven't activated its security certificate.

image

I was able activate it from the thing security page:

image

And than I was able to run the demo program from the board, create connection, publish and receive messages:

image

 

AWS IoT Connection Troubleshooting

 

I wish there is a way to troubleshot AWS IoT connection. Probably I just don't know about it.

 

What helped me a lot is that I've used AWS IoT Linux/Python demo program and it worked perfectly from the first time.

curl https://www.amazontrust.com/repository/AmazonRootCA1.pem > root-CA.crt
python aws-iot-device-sdk-python/samples/basicPubSub/basicPubSub.py -e my-ats.iot.us-east-1.amazonaws.com -r root-CA.crt -c bio2.cert.pem -k bio2.private.key

vlasov01@remote:~/bio2$ python aws-iot-device-sdk-python/samples/basicPubSub/basicPubSub.py -e my-ats.iot.us-east-1.amazonaws.com -r root-CA.crt -c bio2.cert.pem -k bio2.private.key
2020-03-29 22:33:03,311 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Initializing MQTT layer...
2020-03-29 22:33:03,312 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Registering internal event callbacks to MQTT layer...
2020-03-29 22:33:03,313 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - MqttCore initialized
2020-03-29 22:33:03,313 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Client id: basicPubSub
2020-03-29 22:33:03,313 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Protocol version: MQTTv3.1.1
2020-03-29 22:33:03,313 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Authentication type: TLSv1.2 certificate based Mutual Auth.
2020-03-29 22:33:03,314 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring endpoint...
2020-03-29 22:33:03,314 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring certificates...
2020-03-29 22:33:03,314 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring reconnect back off timing...
2020-03-29 22:33:03,314 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Base quiet time: 1.000000 sec
2020-03-29 22:33:03,314 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Max quiet time: 32.000000 sec
2020-03-29 22:33:03,315 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Stable connection time: 20.000000 sec
2020-03-29 22:33:03,315 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring offline requests queueing: max queue size: -1
2020-03-29 22:33:03,316 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring offline requests queue draining interval: 0.500000 sec
2020-03-29 22:33:03,316 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring connect/disconnect time out: 10.000000 sec
2020-03-29 22:33:03,316 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Configuring MQTT operation time out: 5.000000 sec
2020-03-29 22:33:03,317 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Performing sync connect...
2020-03-29 22:33:03,317 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Performing async connect...
2020-03-29 22:33:03,317 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Keep-alive: 600.000000 sec
2020-03-29 22:33:03,318 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Event consuming thread started
2020-03-29 22:33:03,318 - AWSIoTPythonSDK.core.protocol.mqtt_core - DEBUG - Passing in general notification callbacks to internal client...
2020-03-29 22:33:03,318 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Filling in fixed event callbacks: CONNACK, DISCONNECT, MESSAGE
2020-03-29 22:33:03,599 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Starting network I/O thread...
2020-03-29 22:33:03,707 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [connack] event
2020-03-29 22:33:03,707 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [connack] event
2020-03-29 22:33:03,709 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - No need for recovery
2020-03-29 22:33:03,709 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:03,717 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Performing sync subscribe...
2020-03-29 22:33:03,718 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Adding a new subscription record: sdk/test/Python qos: 1
2020-03-29 22:33:03,719 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Filling in custom suback event callback...
2020-03-29 22:33:03,802 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [suback] event
2020-03-29 22:33:03,802 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [suback] event
2020-03-29 22:33:03,802 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:03,803 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - This custom event callback is for pub/sub/unsub, removing it after invocation...
2020-03-29 22:33:05,835 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Performing sync publish...
2020-03-29 22:33:05,837 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Filling in custom puback (QoS>0) event callback...
2020-03-29 22:33:05,905 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [puback] event
2020-03-29 22:33:05,906 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [puback] event
2020-03-29 22:33:05,907 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:05,908 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - This custom event callback is for pub/sub/unsub, removing it after invocation...
2020-03-29 22:33:05,943 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [message] event
2020-03-29 22:33:05,945 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [message] event
Received a new message:
{"message": "Hello World!", "sequence": 0}
from topic:
sdk/test/Python
--------------


2020-03-29 22:33:05,950 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:06,955 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Performing sync publish...
2020-03-29 22:33:06,957 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Filling in custom puback (QoS>0) event callback...
2020-03-29 22:33:07,024 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [puback] event
2020-03-29 22:33:07,025 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [puback] event
2020-03-29 22:33:07,026 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:07,027 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - This custom event callback is for pub/sub/unsub, removing it after invocation...
2020-03-29 22:33:07,055 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [message] event
2020-03-29 22:33:07,057 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [message] event
Received a new message:
{"message": "Hello World!", "sequence": 1}
from topic:
sdk/test/Python
--------------


2020-03-29 22:33:07,061 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:08,073 - AWSIoTPythonSDK.core.protocol.mqtt_core - INFO - Performing sync publish...
2020-03-29 22:33:08,074 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Filling in custom puback (QoS>0) event callback...
2020-03-29 22:33:08,165 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [puback] event
2020-03-29 22:33:08,167 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [puback] event
2020-03-29 22:33:08,168 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - Invoking custom event callback...
2020-03-29 22:33:08,168 - AWSIoTPythonSDK.core.protocol.internal.clients - DEBUG - This custom event callback is for pub/sub/unsub, removing it after invocation...
2020-03-29 22:33:08,172 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Produced [message] event
2020-03-29 22:33:08,174 - AWSIoTPythonSDK.core.protocol.internal.workers - DEBUG - Dispatching [message] event
Received a new message:
{"message": "Hello World!", "sequence": 2}
from topic:
sdk/test/Python
--------------

 

Than I've tried to use it with the thing certificate/private key and it failed. Than I've used the certificate/private key supplied with AWS IoT Linux/Python demo program and my device was able finally connect. So, I've realized that the issue was related to the thing certificate and private key. I've validated them and haven't found any issues:

image

Then I've started reading about management from CLI perspective. This is where I noticed activation step.

  • Sign in to reply

Top Comments

  • vlasov01
    vlasov01 over 6 years ago in reply to neuromodulator +1
    It was working fine for me. There was no issues with the WIFI AP. I was using mtb 2.0 to build and deploy code. I need to test if it is still working with mtb 2.1.
Parents
  • neuromodulator
    neuromodulator over 6 years ago

    Did you experience inconsistent connectivity to the WIFI AP? Sometimes I get the board to connect, others it just doensn't.

    The LF and CR of the log also look quite crappy on my end. Thought it was some race condition, but it appears to be kinda deterministic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neuromodulator
    neuromodulator over 6 years ago

    Did you experience inconsistent connectivity to the WIFI AP? Sometimes I get the board to connect, others it just doensn't.

    The LF and CR of the log also look quite crappy on my end. Thought it was some race condition, but it appears to be kinda deterministic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vlasov01
    vlasov01 over 6 years ago in reply to neuromodulator

    It was working fine for me. There was no issues with the WIFI AP.

    I was using mtb 2.0 to build and deploy code. I need to test if it is still working with mtb 2.1.