Connected Cloud Challenge
  • Challenges & Projects
  • Design Challenges
  • Connected Cloud Challenge
  • More
  • Cancel
Connected Cloud Challenge
Documents Connected Cloud Design Challenge - Winners Announcement
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14phil
  • Date Created: 23 Jun 2020 1:44 PM Date Created
  • Last Updated Last Updated: 23 Jun 2020 4:26 PM
  • Views 4735 views
  • Likes 12 likes
  • Comments 41 comments
Related
Recommended

Connected Cloud Design Challenge - Winners Announcement

I am happy to announce today's Winners of the Connected Cloud Challenge with Cypress

 

After 20+ weeks of designing,Researching, Prototyping, Coding and Testing, 142 Blog Posts, 17 Videos, our Connected Cloud Challenge  has come to a close.

Our challengers were tasked to use the PSoC 6 and Amazon AWS IoT Platform to connect their world!

The judges have rounded up their thoughts on the projects and selected their favorites.


Prizes

Grand Prize

Runner Up

Finisher Prize

image

 

Grand Prize

Lulzbot Mini 2 Desktop 3D Printer*

Valued at $1480

&

A brand new, next-generation PSoCRegistered 6 MCU Dev Kit (to be announced). Be one of the first to try it out!

image

 

Runner up

HTC VIVE Pro Virtual Reality System*

Valued at $1050

&

A brand new, next-generation PSoCRegistered 6 MCU Dev Kit (to be announced). Be one of the first to try it out!

image

 

Finisher Prize

For anyone who completes 10 Blogs and a project with the featured product.

MultiComp Pro Multimeter Set*

Valued at $60

 

Winners of the Connected Cloud Challenge with Cypress and AWS

 

Grand Prize

Super Smart Home by - balearicdynamics
Top Member, Enrico, won us over with his Super Smart Home Autimation project, using the PSoC6 as the main hub to his AWS IoT Smart home. Using cross platform MQTT and AWS for the main infrastructure, creating his own 3D printed cases and remote ESP8266 nodes as well as UI for the PSoC6. The large amount of cross platform inter connectivity helped the judeges select this project as the overall winner.

image


Read All Enricos Blogs Here


Runner Upimageimage

Intelligent Mailbox by -saicheong
Sai comes in second with their Smart Mailbox. This remote mailbox seems fairly simple on first glance but the complexity within really blew the mind of the judges.
Firstly the project would light up and inform you when a letter arrives, this passes the data over AWS to a telegram service, email or SMS, Fairly simple but well done.

We had a 2 week extension at the end of this challenge and some challengers who were finished and downed tools, Sai decided to use the remaining time at the end of the challenge to Train a Neural Network with sounds of dogs playing and barking. Training this mailbox to know if a dog is barking aggressively and then to warn the mail carriers of this.

imageimage

imageimage

 

Read All of Sai's Blogs Here

 

 

Honorable Mentions

These projects won't be winning the top spot prizes but we loved their projects so much we wanted to publicize their amazing work.

 

sami9974

Samyak created a Billboard Rental System. Allowing users to buy advertisement space on a website, AWS would handle the data and the advertisements would be displayed on location for the time period paid for.

imageimageimage

Read Samyaks Blogs Here

 

wanfp97
Wan Created a Smart Pet Watering and Feeding System, including Amazon FreeRTOS and using the Cypress PSoC 6's touch sense to stop the bowl from over filling
imageimage

Read Wans Blogs Here

 

jeromedominic
Jerome created an Amazon Alexa Integrated pill dispenser with remote authorization and voice control using MQTT, AWS and the Cypress PSoC6 as the main controller.



imageimageimage

Read Jerome's Blogs Here

 

 

I want to thank Cypress and Amazon for their amazing support during this challenge as they have worked very closely with the community to produce some amazing projects using the PSoC 6.

Have you enjoyed reading about the PSoC 6 and the products in this challenge, feel free to get your own here:

 

The Kit Options (Choose One)The Specs

image

PSoCRegistered 6 WiFi-BT Pioneer Kit

(CY8CKIT-062-WIFI-BT) from Cypress

 

Buy Pioneer KitBuy Pioneer Kit

  • The ultra-low-power PSoCRegistered 62 MCU that integrates an ArmRegistered CortexRegistered-M4 and Cortex-M0+ onto a single chip and provides up to 1 MB of Flash and 288 KB of SRAM
  • The Murata 1DX Module hosting the Cypress CYW4343W 802.11 b/g/n Wi-Fi + Dual-Mode Bluetooth combo chipset radio
  • TFT display shield board that provides users with a 2.4” TFT display, a light sensor, a 6-axis motion sensor, and a digital microphone
  • PSoC 5LP MCU for program/debug
  • Cypress' CapSenseRegistered capacitive touch sensing enabled buttons and sliders
  • Cypress ExcelonTm-Ultra 4Mbit 108-MHz QSPI nonvolatile F-RAM in an 8-SOIC package
  • An EZ-PDTm CCG3 Type-C power delivery system is also on board and is pre-configured to be able to deliver power from a Type-C port to an on-board header while at the same time charging a 3.7 V lithium-ion polymer battery

image

PSoCRegistered 6 WiFi-BT Prototyping Kit

(CY8CPROTO-062-4343W) from Cypress

 

Buy Prototyping KitBuy Prototyping Kit

  • The ultra-low-power PSoCRegistered 62 MCU that integrates an ArmRegistered CortexRegistered-M4 and Cortex-M0+ onto a single chip and provides up to 2 MB of Flash and 1 MB of SRAM
  • The Murata 1DX Module hosting the Cypress CYW4343W 802.11 b/g/n Wi-Fi + Dual-Mode Bluetooth combo chipset radio
  • PSoC 5LP MCU for program/debug
  • Cypress' CapSenseRegistered capacitive touch sensing enabled buttons and sliders
  • Cypress 512 Mb Quad-SPI NOR Flash device
  • MicroSD card slot
  • PDM microphone and thermistor
  • Digilent PmodTm interface
  • connected cloud
  • cypress psoc 6 ble pioneer kit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 6 years ago +7
    Thank you for the great news! And congratulations to the other winners. Cheers, Enrico BTW... I am extremely curious about what is the new PSoC6. When some extra info can be revealed???
  • balearicdynamics
    balearicdynamics over 6 years ago +7
    Unpacked the prize! (the 3D printer has been converted in a fantastic bunch of cool stuff)
  • Jan Cumps
    Jan Cumps over 6 years ago +5
    Congratulations!
Parents
  • balearicdynamics
    balearicdynamics over 6 years ago

    Unpacked the prize!

    (the 3D printer has been converted in a fantastic bunch of cool stuff)

    imageimageimage

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to balearicdynamics

    Very nice Enrico!.

     

    That mini lathe looks neat.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to luislabmo

    I have just tried to power on it and it works fine. Next week I expect the tools to try making some metal parts, the one that usually I can't do with 3D printer (hehe) or other methods. On the paper, it has a precision of 0.05 that is more than sufficient for most of the cases I will work. The next step is trying to make a metal piece from an Aluminium bar then I will see what happens. Then I already checked, it's not difficult to add a stepper to the manual controls... Another nice too to hack.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to balearicdynamics

    If you can add the stepper to the lateral movement, you can cut custom screw thread with the machine.... If the spindle can be put on very low rotation speed.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to Jan Cumps

    I will add two stepper-motors, also the longitudinal movement. This is used – moving very slow – to make perfect holes in the center of metal stuff with special drill tools for lathes. Instead, for the lateral movement, it is not needed to make a very very slow motion – I mean, this small lathe has the lowest speed 800 rpm that is sufficiently slower, but no need to go slower than this – but it is a question of synching the two movements.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to balearicdynamics

    Yes, it would never produce a precision thread image.

    The lathe at school used the spindle driver to also drive the cutters horizontal movement - via reduction.

    That way, because horizontal movement was a function of rotation speed, you had a guaranteed thread "speed".

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to balearicdynamics

    Yes, it would never produce a precision thread image.

    The lathe at school used the spindle driver to also drive the cutters horizontal movement - via reduction.

    That way, because horizontal movement was a function of rotation speed, you had a guaranteed thread "speed".

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 6 years ago in reply to Jan Cumps

    The hack is a hack... The idea is that this is the structure, and is useful for hand-work. Then motors should be synched, including the spindle motor. With what? An optical encoder (shabaz  hehe).
    I mean, that motorizing it includes many changes, and also a 3 axis controller that should be modified to change the cartesian representation to non-Euclidean space. Nothing easy, but nothing impossible (hopefully)

     

    Enrico