Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Connection Issues
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
  • Author Author: roborob1266
  • Date Created: 10 Aug 2018 2:37 AM Date Created
  • Views 5203 views
  • Likes 6 likes
  • Comments 20 comments
  • arduino mkr1000
  • issues
  • wiring
  • adafruit vs1053 mp3 player
  • 5" touch screen
  • design for a cause - design challenge
  • adafruit ra8875
Related
Recommended

Connection Issues

roborob1266
roborob1266
10 Aug 2018

image

Hello everyone. I was able to get the Adafruit RA8875 to work with the MKR1000.

I was recently able to get the VS1053 (Adafruit Music Maker MP3 Shield) to work with the MKR1000.

The issue is when I connect them together with the MKR1000, I cannot get the MP3 shield to work.
It is not detected with the wiring I am selecting.
I am using hardware SPI so SCK, MISO and MOSI are being used.This is the wiring I am using for the RA module, MP3 Module and the MKR.

I know that the MKR has pins 0 and 1 as the interrupt pins and switching between those doesn't work.

Since I am using the breakout portion of the MP3 player, that is why I connected it to the MKR and it worked.

 

VS1053MKR1000
5V5V
GNDGND
Breakout ResetReset
SCK139
MISO1210
MOSI118
MCS71
DCS65
CardSC44
DRQ30
RA8875MKR1000
5V5V
GNDGND
SCKSCK9
MISOMISO10
MOSIMOSI8
CSCS6
RST2
INTINT3

 

Once I am able to make these all play nicely then I will be able to use the image files and place them on the screen and then learn now to trigger a touch to play the appropriate wav file.

This challenge has really taught me the value of research, which forums do not help at all and trial and error will get you results in the end! It didn't stop Thomas Edison from inventing the light bulb after thousands of tries, it wont stop me either!

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 8 years ago +5
    Hi Rob, If you're developing approximately what I think you're developing, it is really good news. I too am on the side working on a project for autistic children. Quite surprising how little easy-to-make…
  • aspork42
    aspork42 over 8 years ago +4
    Does the VS1053 have a pin labeled just as "CS"? When I look on Adafruit, I see a different looking board than what you have, but it does show a "CS" pin. This is the "select" pin that the master (MKR1000…
  • prashanth.nagendrappa
    prashanth.nagendrappa over 8 years ago +3
    Nice Update Keep going roborob1266
Parents
  • aspork42
    aspork42 over 8 years ago

    Does the VS1053 have a pin labeled just as "CS"? When I look on Adafruit, I see a different looking board than what you have, but it does show a "CS" pin. This is the "select" pin that the master (MKR1000) uses to tell the slave to listen. Each slave must have its own "Chip Select" pin that cannot be shared. (Also call "slave select" or something similar.)

     

    image

     

    The next thing - How are you 'disconnecting' one or the other when you test? Just removing power or removing all wiring? And is all other wiring the same when the they work individually versus all wired in at ones?

    In theory you should be able to have both all wired in, and run a test sketch one time for each board, just modifying the header info for the correct pinout. I would think that just removing power from the slave should effectively disable it so you can test the other board.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to aspork42

    It's not very clear but looks like the pins labelled MCS and DCS here: https://learn.adafruit.com/assets/16643

    go to XCS and XDCS pins in that order, on the VS1053 chip according to the circuit diag here: https://cdn-learn.adafruit.com/assets/assets/000/016/642/original/adafruit_products_schem.png?1400269761

     

    It seems the XCS pin is the chip select for the SPI interface? (chip datasheet: https://www.sparkfun.com/datasheets/Components/SMD/vs1053.pdf  )

    Rob, how are you confirming that the MP3 shield is not detected? If you've not got a 'scope, you can use an LED and a resistor (e.g. 220 ohms) on the CS pin (i.e. MCS I think) to see if it stays permanently lit, or if it briefly flickers to off.

    Also, could it be a supply issue? The display and MP3 shield combined may use more power than expected. Are you running this from USB?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 8 years ago in reply to aspork42

    It's not very clear but looks like the pins labelled MCS and DCS here: https://learn.adafruit.com/assets/16643

    go to XCS and XDCS pins in that order, on the VS1053 chip according to the circuit diag here: https://cdn-learn.adafruit.com/assets/assets/000/016/642/original/adafruit_products_schem.png?1400269761

     

    It seems the XCS pin is the chip select for the SPI interface? (chip datasheet: https://www.sparkfun.com/datasheets/Components/SMD/vs1053.pdf  )

    Rob, how are you confirming that the MP3 shield is not detected? If you've not got a 'scope, you can use an LED and a resistor (e.g. 220 ohms) on the CS pin (i.e. MCS I think) to see if it stays permanently lit, or if it briefly flickers to off.

    Also, could it be a supply issue? The display and MP3 shield combined may use more power than expected. Are you running this from USB?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • roborob1266
    roborob1266 over 8 years ago in reply to shabaz

    Hello Shabaz,

    Here are the scenarios that happened this morning.

    I connect the VS1053 to the MKR - RA8875 is not connected - Audio works fine when I run the simple player sketch. I verify that it is working and detected via the Serial monitor.

    I then connect the RA8875 to the MKR while the VS1053 is connected and it will not display, the back light will not even turn on and the VS1053 will not play an audio file when I run the sketch.

    I run the video sketch I have for touch screen buttons and it will not work.

    I have to disconnect all the cables from the VS1053 in order for the RA8875 to operate after I run the touch screen sketch.

    It seems like powering the RA8875 and VS1053 together with the MKR does not work even with the USB connection connected to the MKR1000.

     

    I can connect the VS1053 to the UNO and power it that way and get the RA8875 to run with the MKR1000 but I am not sure how to make the MKR communicate with the UNO so audio is played when buttons are touched on screen from the RA8875 via the MKR unit. Right now having the MKR as the master and the UNO as the slave is not communicating either from TX/RX or I2C.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to roborob1266

    Hi Rob,

     

    You may need access to a 'scope, but if that is not available, you could try a hack, where you stick an LED across both CS pins with a resistor (say 220 ohms) in series. Since Both CS lines should never be low simultaneously, you should see the LED light up in one direction (you could put two back-to-back).

    If the two LEDs are both permanently off, then that's a sign that something is wrong.. You could try to pick a completely different pin to act as the CS pin on the MKR board, to see what happens. The code would need to select that line, or you'd need to do the selection at the point when the device that it is connected to needs enabling.

    I'm just speculating if it is a CS line issue, it is hard to know for sure.

     

    It could also be a supply issue, for that you'll need to use a multimeter to check the supply rail is still at 5V. Can you check that if possible?

     

    Personally I think it's a lot harder if you use an additional UNO and try to communicate between the two. I would not try that, but it's really your decision. I think it's worth troubleshooting your scenario further, but it requires some way examining the signals, or seeing if you can adapt the code if you suspect there could be some clashes in the drivers perhaps.

     

    Right now, to me, it points to either a chip-select issue, or a power supply issue. But I'm really guessing : ( I don't know for sure.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • roborob1266
    roborob1266 over 8 years ago in reply to shabaz

    HI Shabaz,

    I read online that there is an issue with the SPI section for the MKR1000 where unless you use a tri-state buffer chip, it has a hard time telling one CS pin from another which could be the issue that I am experiencing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to roborob1266

    Hi Rob,

     

    When the microcontroller is acting as a Master, then it's up to the slave devices (i.e. the VS1053 and RA8875 boards) to perform the tri-state operation, not the MKR board.

     

    The MKR board just needs to instruct (by pulling the relevant CS line high) the slave devices to go tri-state on their MISO line. This is why it would be good to closely examine what is happening on your CS lines for the two devices. If the CS lines for both devices are simultaneously low, then that's a very bad thing.

     

    The thing is, you don't need any SPI driver interaction to correctly control CS lines. You can define any connection on the MKR board to act as an output pin, and then write code (i.e. DigitalWrite) to pull the CS lines high or low under your own command, provided you put it at the correct location. It could well be the case that threads are executing that are pulling both CS lines low, That is not a MKR board issue, but could be a software or software driver issue.

     

    This is all speculation though, and a way through this is to check the CS lines using the methods mentioned (ideally oscilloscope, or using LEDs).

    A tri-state buffer chip could be used, but to me it sounds superfluous, unless there is some device-level reason why either of the devices is not going tri-state.

     

    I don't know what the code looks like, but if you're executing a write to the display, it could be worth inserting a delay after that as a test, so that if the display is written in a different thread (I've never used the MKR board, I'm just guessing) then that thread has some time to complete before sending data to the VS chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • roborob1266
    roborob1266 over 8 years ago in reply to shabaz

    Hello,

    All I do is connect the RA8875 and the VS1053 to the MKR board and power it on and neither of them work even before I run any sketches.

    I will try the LED process to see what is going on with the CS lines.