to
Coordinated Universal Time
The World Wide Web
June 27 via World Wide Web EMC Part III: Shielding 13:00-14:00 CST Click here to register Hebberly Ahatlan, Field Applications Engineer, will cover EMC and what it means to you and your designs. EMC Part III introduces shielding materials such as gaskets...
I've read about prints slanting and sliding due to belt loosening and have had that happen to myself, but I am now suffering an unusual setback as prints of my self designed pieces all slant at a continuous slope in the x axis, yet files I download from…
Today, I received my purchased pre-installed Noobs OS. I get a blank screen when I boot my pi2. I can see the files on the sd card when I insert it nto my PC. Also, I want load a single OS onto a another sd card and safe keep my original copy. Could someone…
The scenario I am working on a project where I need to "evolve" several Gizmo2 board to make them specialised for some tasks. In short words the rules are the following Desk unit : This is the most simple model ; it will include a series of peripheral…
Hello All - I just purchase the element14 Pi A+ at microcenter and am having a noise issue with the board. Immediately upon power up the 1/8 output is extremely noisy, to the point that it would be useless for my application (soundfont player) Also there…
Apple probably wanted its newest iPad to be thought of as a hot item, but not like this. Over the weekend, reports began to circulate that the newest iPad, just released on Friday , was becoming physically hot to the touch during use, specifically in…
Hello everyone. I was able to get the Adafruit RA8875 to work with the MKR1000. I was recently able to get the VS1053 (Adafruit Music Maker MP3 Shield) to work with the MKR1000. The issue is when I connect them together with the MKR1000, I cannot get…
So I bought all the components I need to make a PMI2 and put it all together, being sure to measure multiple times so it can be accurate as possible. The only issues Ive had are the electronics, mainly the stepper motors. They're have some slight binding…
Hi there, Im an electronic and im looking for a cheap 3D printer... so in my way in the internet finding it, i've found 2 , the One up , Makible A6.. Comparing them the best option is obviusly the One Up... so i went in the kickstarer page and saw alot…
I think I found another problem I didn't notice before. I have the R-pi hooked up in the prototyping gig I described on another thread ( http://www.element14.com/community/thread/18981?tstart=0 ), currently no keyboard, HDMI monitor, just network and…
I'm new to the element14 community and made up my profile earlyer today. The avatar picture uploader worked great but the profile picture (the one where its recommended to use a picture of oneself) is not working so well. long story short it always says…
Hi, i just bought a CS license from Farnell. But there is a HUGE issue with license delivery 1. I bought the license this week and got it today (24/9/2016) - but license start date is the 20/09/2016 and order date was 23/09/2016?) - are you shorting out…
Hi im making raspberry pi portable.Im using raspberry pi 1 B.Ihave issues with composte video dosent work on raspbian.I tried uncommenting hdmi hotplug and disconected hdmi when booting but it didnt work .If you know a solution please help me thanks for…