Design for a Cause - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Design for a Cause - Design Challenge
  • More
  • Cancel
Design for a Cause - Design Challenge
Blog Week 6 - Calibration and Communication
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
  • Author Author: kyle90
  • Date Created: 22 Aug 2018 4:22 PM Date Created
  • Views 2045 views
  • Likes 4 likes
  • Comments 7 comments
Related
Recommended

Week 6 - Calibration and Communication

kyle90
kyle90
22 Aug 2018

Everything is really starting to come together now! On the fall detection side of things, we built a test rig to hold the accelerometer and a spare Arduino, for calibrating the axes and doing some drop tests. This was constructed from Lego bricks, which have the advantages of being quick to assemble and disassemble, and keeping everything at known right angles.

image

The "X" on the front is to remind us that the positive X axis is in that direction.

 

We also bought a SIM card so that the GSM module can talk to the cell network, and wrote the code that will let the Arduino send and receive data from the GSM module.

image

image

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Nice update on your design challenge project. Good to see that things are moving along. Keep up the good work. Gene
  • kyle90
    kyle90 over 8 years ago in reply to dixonselvan +2
    Hi, thanks for the feedback. We want it to detect if the user falls so that if they are unable to call for help themselves (unconscious, broken bones, etc.) it will automatically send a message to someone…
  • dixonselvan
    dixonselvan over 8 years ago in reply to kyle90 +2
    Thanks for the reply kyle90 Good luck on your project.
Parents
  • dixonselvan
    dixonselvan over 8 years ago

    Hi kyle90

     

    Nice progress on your project. I love the Lego Bricks case and specifically the X and the arrow mark to indicate X axis. I use metal Mechanix sets for fast prototyping case requirements. You can see some examples here Traffic Predictor #5 - Machine Learning and Building a case for the kit , DIY LED Ferris Wheel

     

    Are you sending an SMS in case of a fall? Would you mind letting me know the purpose? You can also see a similar setup for a part of my project here Cue System for Anosmia and Smart WheelChair #6 - Fall and Collision Detection [DIY]  and take reference or let me know in case of any help.

     

    Thanks,

    Dixon Selvan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dixonselvan
    dixonselvan over 8 years ago

    Hi kyle90

     

    Nice progress on your project. I love the Lego Bricks case and specifically the X and the arrow mark to indicate X axis. I use metal Mechanix sets for fast prototyping case requirements. You can see some examples here Traffic Predictor #5 - Machine Learning and Building a case for the kit , DIY LED Ferris Wheel

     

    Are you sending an SMS in case of a fall? Would you mind letting me know the purpose? You can also see a similar setup for a part of my project here Cue System for Anosmia and Smart WheelChair #6 - Fall and Collision Detection [DIY]  and take reference or let me know in case of any help.

     

    Thanks,

    Dixon Selvan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • kyle90
    kyle90 over 8 years ago in reply to dixonselvan

    Hi, thanks for the feedback. We want it to detect if the user falls so that if they are unable to call for help themselves (unconscious, broken bones, etc.) it will automatically send a message to someone who can get help.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 8 years ago in reply to kyle90

    Thanks for the reply kyle90 Good luck on your project.