Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Enchanted Objects Design Challenge - The Woodcutter and the Blacksmith
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
  • Author Author: Workshopshed
  • Date Created: 30 Mar 2015 6:53 AM Date Created
  • Views 2940 views
  • Likes 3 likes
  • Comments 21 comments
  • enchanted_cottage
  • enchanted_objects
Related
Recommended

Enchanted Objects Design Challenge - The Woodcutter and the Blacksmith

Workshopshed
Workshopshed
30 Mar 2015

The Woodcutter

 

Matilda needed some wood for the house extension so she set off through the forest to visit the woodcutter. She found him in a clearing formed by trees that had fallen in the same storm that had damaged the enchanted cottage. "Several trees fell during the storm" said the woodcutter, "but I did not hear them". The wood cutter pointed to the young sapling amongst the fallen trees. "The sapling bends with the wind but the oak breaks" he said. Matilda thought maybe the woodcutter spent a bit too much time on his own.

 

Matilda showed the wood cutter her plans for the basement and rear extension to the enchanted cottage.

image

The woodcutter set about one of the fallen trees and soon had it converted into planks for Matilda's design, she helped him load the into the cart and then headed off to see the blacksmith

image

The Blacksmith

Matilda always liked visiting the Cel the blacksmith as it was always nice and warm in his shop. She showed Cel the plans for the Watt's linkage and the he set about making the first parts.

image

When the tested them the pins were too weak and one snapped off. They both cursed at the wasted time and discussed an alternative. Their second attempt was successful and used a hardened screw to re-enforce the joint.

imageimage

Matilda redesign all of the parts to work this way and left the plans with the Blacksmith who set about making them.

imageimage

There were a few changes to the parts over the next few hours but eventually Matilda has a set of components she was happy with.

image

By the time she had returned home, Hans had finished the repairs to the roof

 

{gallery:width=300,height=400}Roof repairs

image

Roof Glue up

image

Roof battens

image

Roof back on

The next job for Matilda was to put the parts into motion and her thoughts thoughts returned to the words of the woodcutter. Perhaps she thought, rather than directly connecting the servo to her mechanism she could use a springy sapling. Then if anything locked up the sapling would flex rather than causing the servo or mechanism to break.

 

Next Enchanted Objects Design Challenge - Back on the straight and narrow

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago +2
    left the plans with the Blacksmith who set about making them Funny how they are plastic ... are you sure Cel is a blacksmith and not farming it out to some cheap alternative labour source?? Maybe Cel…
  • Workshopshed
    Workshopshed over 11 years ago in reply to mcb1 +2
    I was thinking a springy wire, something like this From RC Boat Rudder Linkage
  • mcb1
    mcb1 over 11 years ago in reply to Workshopshed +2
    That might work as well. Several ways to skin the cat so to speak.... Mark
  • Workshopshed
    Workshopshed over 11 years ago in reply to gadget.iom

    I do have some panels but they are about 10 times the size of the house image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to Workshopshed

    How much would it take to convince Matilda that solar panels on the roof may reduce their energy bills?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to Workshopshed

    At least the lack of battery shouldn't delay development too much. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to gadget.iom

    Yes, am on schedule and the Yun arriving today means that I've no critical path items. Only purchase remaining is for battery power although I do have a miniature 6v lead acid if I get desperate!

    Still plenty to do thought!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago

    I really like mcb1 suggestion of using a servo saver. Didn't even know they existed until today.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>