Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog MagicHat - 01 - Introduction
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
  • Author Author: amgalbu
  • Date Created: 19 Mar 2015 8:23 AM Date Created
  • Views 2060 views
  • Likes 7 likes
  • Comments 10 comments
  • enchanted_objects
  • Health
  • magic_doctor_hat
  • arduino_yun
  • arduino
Related
Recommended

MagicHat - 01 - Introduction

amgalbu
amgalbu
19 Mar 2015

 

One of the most difficult tasks for a doctor is to divert a child attention while trying to make an injection. And what's better than something magic to entertain a child?

 

So for this challenge I thought of building a magic hat.

 

The magic hat will be able to read a child's mind. Under the hood (literally) there will be an health diagnosis system capable of measuring body temperature, heart rate and blood pressure.

 

To add something real magic, the magic hat will speak, recognize speech and move

 

Here is an image that gives an idea of what I'd like to achieve in this challenge

 

image

 

 

 

The magic hat will be made up the following components

 

1. a Arduino Yun board: the core of the magic hat

 

2. a USB sound interface

 

3. a servo control to make the hat bend

 

4. a IR thermal sensor, like the MLX90614. Melexis' MLX90614ESF-BAA is an infrared thermometer designed for non-contact temperature sensing. An internal 17-bit ADC and a powerful DSP contribute to the MLX90614’s high accuracy and resolution. It has a huge number of applications including body temperature measurment and movement detection.

 

5. a blood pressure sensor. This is something experimental I'd like to try... I will start from a photoplethysmographic sensor and build an apparatus for measuring blood pressure using a finger cuff

 

6. an accelerometer: the accelerometer will detect if magic hat is being carried

 

7. a LED bar to simulate the mouth movements

 

8. a battery pack to power everything up. Since the Arduino Yun is powered through a micro USB, I will likely use a smartphone powerpack

 

Here is how the components will be connected

 

image

 

 

The flow of the whole application is shown in this flowchart

 

image

 

 

 

 

 

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago in reply to shabaz +2
    Hi shabaz I was going to use the melexis temperature sensor because it allows a measure with no need to put it in contact with the skin. However the accuracy is not that good (0.164 °C, which is not good…
  • Workshopshed
    Workshopshed over 11 years ago +1
    Ambrogio that is a fantastic idea, I wish the best of luck with the project
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja +1
    Thanks and as a guy smarter (and richer) than me once said, a magichat in every medical office!!
Parents
  • shabaz
    shabaz over 11 years ago

    It is a really cool idea. Lots of uses, perfect for dentists to use with children too! Especially if the children can't speak due to work being done to their teeth.

    I think you could market that - because not only will it entertain the child, but it would provide valuable visual/audio feedback to the dentist if the child is comfortable or not.

    There must be thousands of dentists who would buy that (and they have the money to pay for it ; ).

    Perhaps a non-Melexis sensor (e.g. TI TMP006) may be better though - I always find it difficult working with Melexis even just to get a few samples out of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago

    It is a really cool idea. Lots of uses, perfect for dentists to use with children too! Especially if the children can't speak due to work being done to their teeth.

    I think you could market that - because not only will it entertain the child, but it would provide valuable visual/audio feedback to the dentist if the child is comfortable or not.

    There must be thousands of dentists who would buy that (and they have the money to pay for it ; ).

    Perhaps a non-Melexis sensor (e.g. TI TMP006) may be better though - I always find it difficult working with Melexis even just to get a few samples out of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 11 years ago in reply to shabaz

    Hi shabaz

    I was going to use the melexis temperature sensor because it allows a measure with no need to put it in contact with the skin. However the accuracy is not that good (0.164 °C, which is not good for a medical application where you have an accuracy of 0.1 °C). So I was now oriented towards this sensos

    http://it.farnell.com/ist-innovative-sensor-technology/tsic-506f-to92/sensore-temp-digitale-0-1deg-c/dp/2191826

    which has 0.1 °C accuracy and a 12-bits digital output. What do you think?

     

    cheers

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to shabaz

    hi shabaz

    Actually my initial idea was to put "under the hood" a mind waves detector to read the emotional status. But that was going a bit too expensive to build so I moved to this simplified approach...

     

    cheers

    Ambrogio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to amgalbu

    Hi Ambrogio,

     

    What a fantastic sensor in your post. I didn't realise such accuracy was possible without calibration. Nice that this IST part comes already calibrated.

    I guess two sensors could be possible too, i.e. a high accuracy one, and the non-contact one if it is impractical to use the accurate one.

    Anyway, nice part you've found.