Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog MagicHat - 01 - Introduction
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
  • Author Author: amgalbu
  • Date Created: 19 Mar 2015 8:23 AM Date Created
  • Views 2419 views
  • Likes 7 likes
  • Comments 10 comments
  • enchanted_objects
  • Health
  • magic_doctor_hat
  • arduino_yun
  • arduino
Related
Recommended

MagicHat - 01 - Introduction

amgalbu
amgalbu
19 Mar 2015

 

One of the most difficult tasks for a doctor is to divert a child attention while trying to make an injection. And what's better than something magic to entertain a child?

 

So for this challenge I thought of building a magic hat.

 

The magic hat will be able to read a child's mind. Under the hood (literally) there will be an health diagnosis system capable of measuring body temperature, heart rate and blood pressure.

 

To add something real magic, the magic hat will speak, recognize speech and move

 

Here is an image that gives an idea of what I'd like to achieve in this challenge

 

image

 

 

 

The magic hat will be made up the following components

 

1. a Arduino Yun board: the core of the magic hat

 

2. a USB sound interface

 

3. a servo control to make the hat bend

 

4. a IR thermal sensor, like the MLX90614. Melexis' MLX90614ESF-BAA is an infrared thermometer designed for non-contact temperature sensing. An internal 17-bit ADC and a powerful DSP contribute to the MLX90614’s high accuracy and resolution. It has a huge number of applications including body temperature measurment and movement detection.

 

5. a blood pressure sensor. This is something experimental I'd like to try... I will start from a photoplethysmographic sensor and build an apparatus for measuring blood pressure using a finger cuff

 

6. an accelerometer: the accelerometer will detect if magic hat is being carried

 

7. a LED bar to simulate the mouth movements

 

8. a battery pack to power everything up. Since the Arduino Yun is powered through a micro USB, I will likely use a smartphone powerpack

 

Here is how the components will be connected

 

image

 

 

The flow of the whole application is shown in this flowchart

 

image

 

 

 

 

 

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago in reply to shabaz +2
    Hi shabaz I was going to use the melexis temperature sensor because it allows a measure with no need to put it in contact with the skin. However the accuracy is not that good (0.164 °C, which is not good…
  • Workshopshed
    Workshopshed over 11 years ago +1
    Ambrogio that is a fantastic idea, I wish the best of luck with the project
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja +1
    Thanks and as a guy smarter (and richer) than me once said, a magichat in every medical office!!
Parents
  • tomaja
    tomaja over 11 years ago

    I didn't see this post until now! What a great idea!

    Good luck with this project, it would really be great to see doctors using it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • tomaja
    tomaja over 11 years ago

    I didn't see this post until now! What a great idea!

    Good luck with this project, it would really be great to see doctors using it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja

    Thanks

    and as a guy smarter (and richer) than me once said,  a magichat in every medical office!!