Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog MagicHat - 5 - Blood pressure sensor
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
  • Author Author: amgalbu
  • Date Created: 2 Apr 2015 12:22 PM Date Created
  • Views 1926 views
  • Likes 6 likes
  • Comments 9 comments
  • enchanted_objects
  • pulse_sensor
  • heart-rate
  • magic_doctor_hat
  • arduino
Related
Recommended

MagicHat - 5 - Blood pressure sensor

amgalbu
amgalbu
2 Apr 2015

I made some modifications to the original circuit I talked about in my previous post and made it on a bread board. Here is the resulting circuit

 

image


image

 

I placed my finger on the sensor, and I got a quite clean signal

 

image

The signal is 200 mV peak-to-peak. Since the ADC has a 10 bits resolution over a 5V range, the signal will be read as 80 ADC steps, which should be enough to make heart beat detection easy

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago in reply to Workshopshed +1
    Hi Clark Thanks for your comments!! Actually mi idea was to use the Arduino Yun to detect heart-beat (both IBI and BPM). I think there is enough power in the Atmel328 for that task! My only doubt is wthether…
  • Workshopshed
    Workshopshed over 11 years ago in reply to amgalbu +1
    www.youtube.com/watch
  • amgalbu
    amgalbu over 11 years ago in reply to amgalbu +1
    Sorry, Arduino Yun has a Atmel324
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    I was watching the EEV blog the other day and Dave was looking a.t an old speach recognition circuit. That used a comparator to turn audio into a square wave and the frequency was read directly via a digital pin on the microcontroller. Obviously if you are using the SAM to analyse the signal you might do that in software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to Workshopshed

    Hi Clark

    Thanks for your comments!!

    Actually mi idea was to use the Arduino Yun to detect heart-beat (both IBI and BPM). I think there is enough power in the Atmel328 for that task!

    My only doubt is wthether to increase gain or not... during my tests I saw that noise increases too, so I think what you see on the scope I the best tradeoff I can currently get. Probably a two-stages amplifier would perform much better


    Cheers

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to amgalbu

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to Workshopshed

    http://www.bizapedia.com/ca/VOICE-CONTROL-PRODUCTS-INC.html a listing for the company he mentioned for the chip. It basically went defunct!

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to amgalbu

    Sorry, Arduino Yun has a Atmel324

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to amgalbu

    Yes, a bit more RAM than the Uno and it behaves more like the Leonardo in that it does not have a separate USB chip so you need to watch resets.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to amgalbu

    Yes, a bit more RAM than the Uno and it behaves more like the Leonardo in that it does not have a separate USB chip so you need to watch resets.