Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running
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
  • Author Author: Jan Cumps
  • Date Created: 11 Apr 2015 8:17 AM Date Created
  • Views 1953 views
  • Likes 2 likes
  • Comments 7 comments
  • sama5d4
  • enchanted_player
  • enchanted_objects
  • xplained_ultra
  • atmel
Related
Recommended

Review 5: Atmel SMART SAMA5D4 Xplained Ultra - TCP/IP running

Jan Cumps
Jan Cumps
11 Apr 2015

I've blogged about my first steps with the kit, Review 1: Unboxing and First Steps.

The second review was on cross compilation on a Windows machine: Review 2: Building the Libraries from Source

 

image

 

This time I connected the board to my home network.

That wasn't difficult at all.

At first I plugged the network cable from router to board while it had already booted.

The network was detected:

 

Oct 30 08:29:16 sama5d4-xplained kernel: macb f8020000.ethernet eth0: link up (100/Full)

 

I didn't get a lease. When I asked linux what my  ip address was, I only got the localhost:

 

root@sama5d4-xplained:~# ip addr show
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc pfifo_fast state UP group default qlen 1000
    link/ether 2a:30:59:a4:17:10 brd ff:ff:ff:ff:ff:ff

 

 

A simple reboot with the cable connected gave me an ip address

 

root@sama5d4-xplained:~# /sbin/ifconfig
eth0      Link encap:Ethernet  HWaddr 96:73:72:46:14:ab
          inet addr:192.168.1.50  Bcast:0.0.0.0  Mask:255.255.255.0
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:30 errors:0 dropped:0 overruns:0 frame:0
          TX packets:4 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:2375 (2.3 KiB)  TX bytes:788 (788.0 B)
          Interrupt:22


lo        Link encap:Local Loopback
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:10 errors:0 dropped:0 overruns:0 frame:0
          TX packets:10 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:700 (700.0 B)  TX bytes:700 (700.0 B)

 

I was also able to ping other computers in  my network:

 

root@sama5d4-xplained:~# ping 192.168.1.27
PING 192.168.1.27 (192.168.1.27) 56(84) bytes of data.
64 bytes from 192.168.1.27: icmp_seq=1 ttl=128 time=91.3 ms
64 bytes from 192.168.1.27: icmp_seq=2 ttl=128 time=4.80 ms
64 bytes from 192.168.1.27: icmp_seq=3 ttl=128 time=2.83 ms

 

and the board shows up on my router's status page

image

 

I was able to connect to the board via a browser from another pc. It shows an "It works!" message (see the first picture).

 

Next Steps:

 

I couldn't get a telnet or ssh session into the board yet. Putty says "Network error: Connection refused"

I'll have to do some more digging to see how I can get that to work on the distro that's on the board, and what I need to do to get this running.

 

This may be my next step up in getting my cross-compiled programs installed and running on the linux distro.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Jan Cumps +2
    Hooray: SSH works with that HTMI image Thanks clem57 and Robert Peter Oakes !
  • clem57
    clem57 over 11 years ago +1
    I flashed the HDMI demo per Robert Peter Oakes suggestion and I get into SAMA5D4 ok. Not sure why you could not? Here is my details: 3.10.1+ #1 linux on Nov 5 2014 Clem
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to clem57 +1
    clem57 , you have that HDMI demo loaded, and you have ssh running on that, right? On that headless distro I'm using the openssh daemon seems to be missing: cat /etc/ssh/sshd_config|more # override default…
Parents
  • clem57
    clem57 over 11 years ago

    You are right... transcription error

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago

    You are right... transcription error