Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1
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
  • Author Author: Jan Cumps
  • Date Created: 20 May 2015 7:08 PM Date Created
  • Views 1687 views
  • Likes 2 likes
  • Comments 7 comments
  • sama5d4
  • enchanted_player
  • enchanted_objects
  • trigger
  • buffer
  • adc
  • xplained_ultra
  • atmel
Related
Recommended

Review 9a: Atmel SMART SAMA5D4 Xplained Ultra - Set up ADC Buffer with Hardware Trigger Part 1

Jan Cumps
Jan Cumps
20 May 2015

I'm trying the Buffer and Hardware Trigger  capabilities of the SAMA5D4.

I followed the instructions on IioAdcDriver < Linux4SAM < TWiki, but was struggling with one particular command.

I raised a topic on tha at91.com forum. And resolved it myself.

Sometimes writing down your problem leads to the solution.

image

 

Instructible

 

You can read my topic on the at91 site to see where I was in trouble.  (jc: At the time of posting this blog, I didn't know yet that I would get the at91.com treatment)
In this blog, I'll post the how-to.

 

Poky (Yocto Project Reference Distro) 1.6.1 sama5d4-xplained /dev/ttyS0


sama5d4-xplained login: root
root@sama5d4-xplained:~# echo 1 > /sys/bus/iio/devices/iio:device0/scan_elements/in_voltage0_en
root@sama5d4-xplained:~# echo "fc034000.adc-dev0-continuous" > /sys/bus/iio/devices/iio:device0/trigger/current_trigger
root@sama5d4-xplained:~# echo 100 > /sys/bus/iio/devices/iio:device0/buffer/length
root@sama5d4-xplained:~# echo 1 > /sys/bus/iio/devices/iio:device0/buffer/enable
root@sama5d4-xplained:~#

 

This will start the process. The ADC will now fill the character device /dev/iio:device0 with data.

 

How did I get the magic name "fc034000.adc-dev0-continuous"? It's different than the name "at91_adc-dev0-external" used in the AT91.com instructions.

By fiddling around a lot, and then by submitting the command

 

 

root@sama5d4-xplained:/sys/bus/iio/devices/trigger0# cat name
fc034000.adc-dev0-continuous

 

I still have to write a program that reads the character device.

I have already checked the source of drivers/staging/iio/Documentation/generic_buffer.c but I haven't been successful in compiling it yet.

I'll also need to learn how I can set the sampling speed.

I'd like to get 128 samples in 3.86ms. Check my previous post to understand why.


I hope that by putting this example here, I can help fellow developers started with the on-board ADC.

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +2
    I did search, and I did find that post. Go read it: http://www.at91.com/discussions/viewtopic.php/f,33/t,24631.html It's difficult to follow because the wits overtones are bigger than the content. It's…
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps +2
    Your efforts are valued even if not by the AT91 crew.
  • Jan Cumps
    Jan Cumps over 11 years ago +1
    I held of posting to at91.com for a long time, because often the tone used. Once I started posting a few days ago, I set a counter for myself on how long it would take for blue_z to come in with a you…
Parents
  • Jan Cumps
    Jan Cumps over 11 years ago

    I held of posting to at91.com for a long time, because often the tone used.

    Once I started posting a few days ago, I set a counter for myself on how long it would take for blue_z to come in with a you should have.

    8 posts.

     

    It feels as if they don't want fans.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 11 years ago

    I held of posting to at91.com for a long time, because often the tone used.

    Once I started posting a few days ago, I set a counter for myself on how long it would take for blue_z to come in with a you should have.

    8 posts.

     

    It feels as if they don't want fans.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    The problem with a new topic area is you don't know what to search for and you don't always understand which cases are similar and which are nothing to do with it.

    I won't be joining the Blue_z fan club either....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    I did search, and I did find that post.

    Go read it: http://www.at91.com/discussions/viewtopic.php/f,33/t,24631.html

    It's difficult to follow because the wits overtones are bigger than the content.

     

    It's a theme. The user after me who posted a question got this treatement:

     

    image

    If that documentation would be up to the mark, I could understand that.

    But it isn't up to the mark.As someone learning the subject, you're not helped by the document, and ridiculed away by the community.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    Still no joy on the at91.com forum.

    How is there ever going to evolve a happy and thriving community from that??

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to Jan Cumps

    That does raise an interesting question about what actually is a "distribution".

     

    I suspect you've got their backs up as you've not followed their "rules" for getting things built. These rules are of course not written down and are only passed on to the worthy and can be changed at will....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    I don't need their backs. I really don't.

    At the end of this exercise I want a nice design where this board plays a significant role.

    But then again, I might just unplug it and put it back in its box if that's how they value the efforts here.