Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The Genie's Day Brightens
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
  • Author Author: RParkerE
  • Date Created: 22 May 2015 9:12 PM Date Created
  • Views 2722 views
  • Likes 4 likes
  • Comments 14 comments
  • enchanted_objects
  • mini_automator
Related
Recommended

The Genie's Day Brightens

RParkerE
RParkerE
22 May 2015

The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done, due to the unfortunate consequences of doing your electrical work in the rain, but today the sun peeked out from behind the clouds and shone with the brightness of 2000-2500 lumen. It was magnificent! However, shortly after its arrival, the clouds took over again . But while the sun was out the genie made headway on his electrical wiring of his sweet new crib. He set the power supply to roughly thirty volts and tested out his lights to see if they worked.

                                                                       imageimage

And it worked! How excited the genie was! This was a huge step in the right direction with the build of his new pad. Now all that was needed to be done was wire it all up to his sweet new dimmer and you could call him Xzibit Jr.

                                                                                                      image

WAIT! There is no light!!!! What in the world is going on? No explosions, check. No fire or smoke, check. Then what? The genie checked the voltage coming out and the light intensity and found:

                                                                  imageimage

But that doesn’t make sense! 30 Volts in and only a 100th of that out? How could this be? The genie has yet to figure this out, but he will be working diligently over the weekend to figure out a solution!

                                                                                   

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to Jan Cumps +3
    Jan Cumps You wouldn't be the first or last to miss something in a post ... You raised a very good pint about the meter though. I wonder if someone who has a working LED can do some checking using a simple…
  • RParkerE
    RParkerE over 11 years ago in reply to mcb1 +3
    I found the culprit and it was much simpler than assumed. I had a poor connection, after I soldered the pins it worked perfectly fine. I am working on my next update now
  • Jan Cumps
    Jan Cumps over 11 years ago +2
    The week was full of rain and clouds for the poor genie all week. Unable to leave his house and make any progress on the things that needed to get done, We seem to have the opposite way of working . I…
Parents
  • ipv1
    ipv1 over 11 years ago

    I think there might be something wrong in the code. The link to my library is https://github.com/inderpreet/infineonrgb_shield and it can be downloaded as a zip and pasted to your project's 'libraries' folder. Restart Arduino and you should see an additional example called lamp test. If you have an RGB LED Strip, it should cycle through possible colors. In case you have a single LED, then it will vary the brightness the LED.

    Hope this help. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RParkerE
    RParkerE over 11 years ago in reply to ipv1

    So I tried your code as well as the code Infineon provides. And for some reason I am unable to enter the loop function, it will not exit out of the setup. When using your code I even attempted to comment out the entire setup method and run it and it still will not reach the loop function I am very confused.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • RParkerE
    RParkerE over 11 years ago in reply to ipv1

    So I tried your code as well as the code Infineon provides. And for some reason I am unable to enter the loop function, it will not exit out of the setup. When using your code I even attempted to comment out the entire setup method and run it and it still will not reach the loop function I am very confused.