Enchanted Objects
  • Challenges & Projects
  • Design Challenges
  • Enchanted Objects
  • More
  • Cancel
Enchanted Objects
Blog The kits are here, Its Time to start
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
  • Author Author: iayanpahwa
  • Date Created: 3 Apr 2015 6:28 AM Date Created
  • Views 1203 views
  • Likes 5 likes
  • Comments 10 comments
  • enchanted_objects
  • enchanted_iot_devices
Related
Recommended

The kits are here, Its Time to start

iayanpahwa
iayanpahwa
3 Apr 2015

I received my kits today, Finally I can start with my first module of Enchanted Wardrobe. It would be around the Yun.

P.S the servo is quiet big, I got an idea to use it wisely image ,@STAY TUNED! for more.image

Thanks Element14 once again...

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed +1
    Here's the review and a test bed: Review 3: Digital Continuous Rotation (360°) Servo . My next challenge is to find a nifty way to use this type of motor. I wasn't expecting a continuous servo. It's surprises…
Parents
  • Workshopshed
    Workshopshed over 11 years ago

    The servo has got a bit of power to it, in my test yesterday it seemed to rotate about 380° when I ran the 0 to 180° sweep code into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to Workshopshed

    Could be a timing issue? You can try the Arduino - ServoWriteMicroseconds command based on the values in the datasheet if mentioned, see if that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to fvan

    I suspect that attaching it with a min and max would work.

     

    servo.attach(pin, min, max)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 11 years ago in reply to fvan

    I suspect that attaching it with a min and max would work.

     

    servo.attach(pin, min, max)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 11 years ago in reply to Workshopshed

    I'm still learning about this, but these servos work differently.

     

    If you write 90 to them, they stop, in the current position, not in a fixed 0 point.

    A value lower than 90: turn left. The lower the value, the faster the speed.

    A value higher than 90: turn right The higer the value, the faster the speed.