• Products and Partners
    Products and Partners
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
Experimenting with Current Sense Amplifiers
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Current Sense Amplifiers
  • More
  • Cancel
Experimenting with Current Sense Amplifiers
Documents Experimenting with Current Sense Amplifiers Challengers
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 28 Mar 2022 9:03 PM Date Created
  • Last Updated Last Updated: 29 Mar 2022 1:57 PM
  • Views 3031 views
  • Likes 7 likes
  • Comments 5 comments
Related
Recommended

Experimenting with Current Sense Amplifiers Challengers

profile image sensors
Experimenting with Current Sense Amplifiers

About Competition | Blogging | Example Application | Resources | The Dates | The Prizes | The Kit | The Judges | Terms & Conditions | The Challengers

Welcome to the Experimenting with Current Sense Amplifiers challengers page!

Our Experimenting with Current Sense Amplifiers Competition a(n) collaboration/association with Maxim Integrated, has now launched.  The 10 challengers will use the current sense amplifiers kit to experiment use, application, response, and more.  These Challengers will receive a Challenger Kit for FREE.

 

Please join us in congratulating the official sponsored Challengers.  We look forward to reading all your initial blogs introducing your project designs.


aspork42 | colporteur | Gough Lui | guillengap | milosrasic98 | misaz | taifur | ujjwalrathod00700 | vinayyn | vishwasn


Current Monitoring for safer 3D Printers

aspork42's project blogs


Model Train Block Detection Using Current Sense

colporteur's project blogs


A Bench Supply Current Monitoring Upgrade

Gough Lui's project blogs


High Precision Calibration of Piezoresistive Pressure Sensors with the MAX40080

guillengap's project blogs


Rover Motor Control

milosrasic98's project blogs


USB Type-C PD Monitoring

misaz's project blogs


Smart Power Bank Controller

taifur's project blogs


Tuning the Parameters for Optimum Use of MAX40080

ujjwalrathod00700's project blogs


Electrical Bicycle Battery Consumption Monitor and Pedal Assistant Guiding System

vinayyn's project blogs


Predictive Maintenance of High Speed Telecom Equipments

vishwasn's project blogs


Congratulations to all our selected challengers!

 

Good Luck Everyone!

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • misaz
    misaz over 4 years ago in reply to zst123 +1
    Sensor is sensing at high speed but output speed is limited by I2C speed. See datasheet for more details, calculations and limits. TLDR version is that chip can communicate at super fast 3.4 MHz I2C, but…
  • dougw
    dougw over 4 years ago +1
    Congratulations to the challengers. Some interesting projects. Looking forward to see how they pan out.
  • zst123
    zst123 over 4 years ago in reply to misaz +1
    Oh yes I didn't think about it. Indeed the datasheet does have a nice chart. 60ksps will be the fastest for real-time streaming of data. Nevertheless, there are some features that may still make it…
Parents
  • zst123
    zst123 over 4 years ago

    Congratulations to the challangers. I submitted a last minute proposal and didn't have time to think of convincing enough solution.
    Looking forward to the blogs. I'm particularly interested and hope to see some tests on the high speed capabilities of the MAX40080.
    Seems like it can sample up to 1 Msps and possibly can capture some current transients in detail. Open mouth

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • misaz
    misaz over 4 years ago in reply to zst123

    Sensor is sensing at high speed but output speed is limited by I2C speed. See datasheet for more details, calculations and limits. TLDR version is that chip can communicate at super fast 3.4 MHz I2C, but very few constrollers supports this. Even on Raspberry Pi it will be very tricky to configure I2C controller to run on this speed. You cant read more than about 60k samples over I2C (60k is maximum at 2.88 MHz I2C bus calculated in datasheet at page 34). High sampling rate is used for averaging (digital filter) multiple samples (up to 128) to one output. Datasheet contains much more calcualtions and estimations about this, but RAW 1 MSPS is definaly impossible to get from this.

    It would be nice to see some details. I think that even with filtering enabled some details could be seen but main purpose of this chip is to monitor long term average consumption. It has some peak related features like comparators which can analyze every of 1 milion samples per second, but this in-chip feature and it is hard to get all of these measured values out of this due to serial bus choice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • misaz
    misaz over 4 years ago in reply to zst123

    Sensor is sensing at high speed but output speed is limited by I2C speed. See datasheet for more details, calculations and limits. TLDR version is that chip can communicate at super fast 3.4 MHz I2C, but very few constrollers supports this. Even on Raspberry Pi it will be very tricky to configure I2C controller to run on this speed. You cant read more than about 60k samples over I2C (60k is maximum at 2.88 MHz I2C bus calculated in datasheet at page 34). High sampling rate is used for averaging (digital filter) multiple samples (up to 128) to one output. Datasheet contains much more calcualtions and estimations about this, but RAW 1 MSPS is definaly impossible to get from this.

    It would be nice to see some details. I think that even with filtering enabled some details could be seen but main purpose of this chip is to monitor long term average consumption. It has some peak related features like comparators which can analyze every of 1 milion samples per second, but this in-chip feature and it is hard to get all of these measured values out of this due to serial bus choice.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • zst123
    zst123 over 4 years ago in reply to misaz

    Oh yes I didn't think about it. Indeed the datasheet does have a nice chart. 60ksps will be the fastest for real-time streaming of data.

    image

    Nevertheless, there are some features that may still make it work, like comparators you mentioned. Perhaps the last 64 samples can be saved upon detecting a current transient. But at 1 Msps it would mean only 64us worth Thinking

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aspork42
    aspork42 over 4 years ago in reply to zst123

    I'm hoping to capture some high-speed transients with my project. Don't know how much success I'll have though.