Experimenting with Extreme Environments
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Extreme Environments
  • More
  • Cancel
Experimenting with Extreme Environments
Forum Driving the LCD - share your experience
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Extreme Environments to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 37 subscribers
  • Views 6761 views
  • Users 0 members are here
Related

Driving the LCD - share your experience

Anthocyanina
Anthocyanina over 2 years ago

Hi! So, I've been working on the software for this challenge and have reached the point where i need to figure out the LCD. The datasheet has a character map and and the addresses for the position of each character. I don't have much experience with driving LCDs so I'm struggling with where to start. Have any of you figured out the LCD yet? 

I found a couple threads on the arduino forum that talk about this display, with people saying you could use the HD44780 libraries, or similar to drive it. I'll be trying that with an arduino board first, but still would like to hear about your experience with this display so far. 

Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 2 years ago in reply to BigG +5
    This one is even simpler.. github.com/.../cfah2004ac community.element14.com/.../IMG_5F00_1443.mov
  • javagoza
    javagoza over 2 years ago in reply to jc2048 +5
    jc2048 A quick adaptation of your script. Works! Thanks for sharing! from smbus2 import SMBus LCD_CLEARDISPLAY = 0x01 LCD_FUNCTIONSET_4LINE_5x8DOTS_BITMODE = 0x38 LCD_DISPLAYCONTROL_ON = 0x0C LCD_ENTRYMODESET_LEFT…
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to shabaz +4
    update time! when i soldered the board to the LCD, which also served as an I2C breakout board, the flux residue was so hard to clean, i couldn't get it all out. I decided to remove that board, which i…
Parents
  • JWx
    JWx over 2 years ago

    I think that HD44780 is pretty standard, but - as you have written - driven mainly from small MCUs 

    Here is some example of using from Raspberry Pi:

    https://tutorials-raspberrypi.com/raspberry-pi-lcd-display-16x2-characters-display-hd44780/?utm_content=cmp-true

    didn't tried it but looks as one would expect it to look...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 2 years ago

    I think that HD44780 is pretty standard, but - as you have written - driven mainly from small MCUs 

    Here is some example of using from Raspberry Pi:

    https://tutorials-raspberrypi.com/raspberry-pi-lcd-display-16x2-characters-display-hd44780/?utm_content=cmp-true

    didn't tried it but looks as one would expect it to look...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Anthocyanina
    Anthocyanina over 2 years ago in reply to JWx

    Thanks! yeah, the thing is, the LCD from the kit doesn't use an HD44780, but the arduino forum posts i found mention it could be driven as if it was the HD44780. This LCD doesn't appear to be commonly used by hobbyists, so there isn't much out there on practical implementations of drivers for it

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 2 years ago in reply to Anthocyanina

    ok - sorry, I have only today got my kit so I didn't check the documentation yet.

    AFAIK HD44780 is considered some sort of standard, with many compatible chipsets. Our LCD seems to be based on/compatible with RW1063 ("For full design functionality, please use this specification in conjunction with the RW1063 specification. (Provided Separately)") - but, according to the datasheet, this driver is 2x8 character max, so maybe some variation of it is installed.

    RW1063  seems to have many interfaces: parallel 4b/8b, serial SPI and I2C, of which our module uses I2C

    https://www.crystalfontz.com/controllers/datasheet-viewer.php?id=227

    https://www.sparkfun.com/datasheets/LCD/HD44780.pdf

    After quick checking, RW1063 parallel interface looks similar to HD44780, so there is a good chance it can be driven with I2C HD44780 Arduino library...