Experimenting with Inductors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Inductors
  • More
  • Cancel
Experimenting with Inductors
Blog Experiment With Inductor : RF Harvesting
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
  • Author Author: kurst811
  • Date Created: 11 Feb 2020 8:06 AM Date Created
  • Views 1816 views
  • Likes 7 likes
  • Comments 2 comments
Related
Recommended

Experiment With Inductor : RF Harvesting

kurst811
kurst811
11 Feb 2020

Introduction

 

The ever-increasing use of wireless devices, such as mobile phones, computing, and remote sensing systems, have led to increased demand and dependence on the use of batteries.One of the market challenges is the potential reduction of large batteries and new power management systems to improve device efficiency. One possibility is to extract energy from the environment to recharge a battery or to directly power the electronic device. RF energy harvesting uses the idea of capturing transmitted electromagnetic waves and storing them for later use. In this experiment I will try different Inductor and see how it will impact the energy amount energy production.

 

image

 

Circuit

 

image

The above circuit is intended to use for this experiment to harvest RF energy. The antenna, capacitor and rectifier diode will stay constant for this experiment while the inductor will be vary. The DC output will be measure using the provided multimeter from the kit.

 

Materials

 

For this experiment, I am going to use the following antenna from this kit https://www.amazon.com/gp/product/B081BD4KG7/ref=ppx_yo_dt_b_asin_title_o01_s00?ie=UTF8&psc=1 . This is your typical antenna that is inside an wireless charger. From research, the antenna are optimize to receive/transmit rf signal.

 

image

 

For the rectifier diode, I am going to use the SMS7630-061 RF diode. These diode low current threshold which are ideal in RF harvesting circuit since the amount of energy circuit get going be low generally.

image

As oppose to the diode and antenna, the capacitor is not as important in this circuit so can be anything as long as it reasonable. So i decided to chose 47uF 25V Electrolytic Capacitor. This might be change in the future, but this is the current capacitor for now.

 

image

 

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +2
    It will be interesting to see what you can achieve with this arrangement. My experience with energy harvesting was that the amount of energy captured was so small that the analogue side of the electronics…
  • three-phase
    three-phase over 6 years ago +2
    You are only using a half-wave rectifier in your circuit, would you not be able to harvest more power by switching to full-wave rectification? Good luck with your experiments. Kind regards
Parents
  • three-phase
    three-phase over 6 years ago

    You are only using a half-wave rectifier in your circuit, would you not be able to harvest more power by switching to full-wave rectification? Good luck with your experiments.

     

    Kind regards

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • three-phase
    three-phase over 6 years ago

    You are only using a half-wave rectifier in your circuit, would you not be able to harvest more power by switching to full-wave rectification? Good luck with your experiments.

     

    Kind regards