Experimenting with Thermal Switches
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermal Switches
  • More
  • Cancel
Experimenting with Thermal Switches
Challenge Blog Blog #1: LED Life Booster/Extender
  • Challenge Blog
  • Forum
  • Documents
  • Files
  • RoadTests
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: karthikrajagopal
  • Date Created: 30 Jan 2022 11:28 AM Date Created
  • Views 3176 views
  • Likes 10 likes
  • Comments 5 comments
  • thermal switch
  • kemet
  • reed switches
  • experimenting with Thermal Switches
Related
Recommended

Blog #1: LED Life Booster/Extender

karthikrajagopal
karthikrajagopal
30 Jan 2022

Self-Intro:

I am Karthik Rajagopal, pursuing my UG course on Electronic Engineering. I am currently working as a Hardware Engineer in a Start-up company as a part of my Internship. I have come across a lot of designs and design constraints  in electronics which has led me to learn further and expand my knowledge in Circuit designing.  Keeping up with the present-day technology is one of the key aspects that has helped me progress.

My experience with Thermal Switches:

Though my field of work does not involve much of power electronics, I have found many situations which needed the application of Thermistors and Thermal switches. One such application I have worked with is a battery  charger. The popular use of Thermistors for soft starting was needed in that circuit. Another application was to have 3 stages of controlled heating in a water heater which was accomplished by  Thermal Switches. Since they have a fixed cut off temperature and can directly be wired up to mains voltage, the whole design cost drastically reduced. A simple network of 5 to 6 thermal switches were used to create heating stages with two thresholds.

                                   image

Problem in current technology:

I recently came across a post about the evolution of LED technology from just being an indicator light to the wide spectrum of applications  it is currently used in. Among those, using them as lighting solution has a good impact on our environment compared to the conventional CFL and Tungsten based  lighting.

While having a better luminous flux to current ratio, the life of those LEDs is limited by a few factors. One such factor is heat. With time, the heat in the LED lamps we use reach a temperature which when operated in the same condition affects the life of the LED bulb.

image

image

Source: https://www.agcled.com/blog/the-application-of-outdoor-led-lights-in-cold-places.html

My Solution and Test Procedure:

My solution to the above problem is to switch between two sets of lighting panel inside the same unit based on heat. This will ensure a better LED life while also maintaining the brightness after switching. The switching will be done by the Thermal switches provided by KEMET.

The threshold temperature will be identified and an appropriate switch will be attached to the heat sink of the LED panels.

image

The circuit will be utilizing a pair of Thermal Switches for each LED strip. This is done to ensure a smooth transition from LED1 to LED2 after reaching the threshold.

The Microcontroller (An Arduino in my case) will take care of the timing aspects in switching.

 

KEMET Switches:

image

The kit of 11 Thermal Switches was very well packed and labelled. I will be testing out the thermal switches with Curie temperature from  30°C to 90°C. Based on hysteresis of the switches, the cut off temperature and timing will be decided.

                                                                                                                                        Blog #2>

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 4 years ago +1
    That seems like an interesting proposal, however, I'm not sure that this is the best idea. One reason is that simply turning the second panel on while turning the first panel off is going to result in…
Parents
  • navadeepganeshu
    navadeepganeshu over 4 years ago

    Great plan karthikrajagopal! LED parts are tortured very much by their own heat....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • navadeepganeshu
    navadeepganeshu over 4 years ago

    Great plan karthikrajagopal! LED parts are tortured very much by their own heat....