Experimenting with Thermistors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Thermistors
  • More
  • Cancel
Experimenting with Thermistors
Forum Soldering Nickel Plated Copper
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 5 subscribers
  • Views 6199 views
  • Users 0 members are here
Related

Soldering Nickel Plated Copper

scottiebabe
scottiebabe over 4 years ago

Soft 404

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago +4
    There's a trick to deal with this type of wires: preheat the join with the iron, usual temperature put solder on the wire, near the landing pad and close to where the iron touches it. let that…
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to scottiebabe +4
    Sounds like the nickel plated kind. They really don't behave like normal stranded wire. You have to lure the solder in like the Pied Piper of Hamelin.
  • rsjawale24
    rsjawale24 over 4 years ago +4
    I think the large copper plane is also taking up the heat from the soldering iron. Just a small copper pad and a higher temperature may help. I would have tried scraping off the nickle from the wire before…
Parents
  • ntewinkel
    0 ntewinkel over 4 years ago

    Oh haha, I just noticed your post now, AFTER soldering them all... and yes I did run into some oddities. I found it was not too bad though, when I used my older paste type flux instead of the newer "no-clean" flux-pen. Maybe the older type of flux has a bit more bite to it Smiley

    I was also just soldering to thin wires, so I guess it all got hot more quickly.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 4 years ago

    Oh haha, I just noticed your post now, AFTER soldering them all... and yes I did run into some oddities. I found it was not too bad though, when I used my older paste type flux instead of the newer "no-clean" flux-pen. Maybe the older type of flux has a bit more bite to it Smiley

    I was also just soldering to thin wires, so I guess it all got hot more quickly.