Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Blog Underwater Camera Test
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 29 May 2023 4:13 AM Date Created
  • Views 1557 views
  • Likes 10 likes
  • Comments 5 comments
  • dougw
  • hammond ip68 enclosure
  • amphenol ip67 connectors
  • experimenting with Waterproof Connectors
  • immersion test
  • lattePanda V1
Related
Recommended

Underwater Camera Test

dougw
dougw
29 May 2023

Intro

This blog highlights the main objective of this project, which is to experiment with the waterproof characteristics of Amphenol connectors and Hammond Manufacturing enclosures.

A camera is built into the box which also features a suite of Amphenol waterproof bulkhead connectors. The camera is not waterproof but the Hammond box keeps it dry and provides a clear window to shoot video through.

This Build and Test Segment

I spent some time 3D printing a pole mount for a battery and even a 3D printed tripod adapter for some video lighting to help shoot in a bathroom.

The mini HDMI cable did not arrive, so I had to use a bigger LCD (because it has a full size HDMI connector) mounted on a separate tripod.

After doing all the work and  making a very nice pole-mount for the LattePanda and display, ended up shooting the demo with the LattePanda and a new display sitting on a table beside the pole.

Demo

This test shows the camera, connected to a LattePanda, recording video underwater:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Discussion

You don't have to worry about losing this camera underwater - it floats.

It has been a struggle to get through the main objectives of this project due to illness. I couldn't even get the initial blog together before its deadline, but the system is working well now and both the Hammond enclosure and the Amphenol connectors are proving to be nicely waterproof.

As can be seen in the video, I trusted the ingress protection capabilities of the enclosure and connectors enough to put a running camera in the case, and I was not disappointed.

The case may look big, bulky and heavy, but the pole is light weight carbon composite and when the case is face down on the water it is totally buoyant so the whole system feels weightless. When it goes in vertically, you have to actually push down a bit to get the camera underwater.

The big display I substiituted in was great, but it would have been better if it was a touch screen, which would allow operation without the wireless touchpad/keyboard.

If you think you recognize the object in the tub, let everyone know in the comments below.

Next Steps

The main objectives are complete, but if I can scrounge a mini HDMI cable, I will do a quick blog on a fully mobile version of the underwater camera system.

There will be another blog to wrap up the project.

Links:

 Sub-Surface WebCam 

 Waterproof Connectors - Camera Build 

 Pole Mechanism for the Waterproof Camera 

LattePanda and LCD Pole -Mounted Chassis

Underwater Camera Test

Hammond and Amphenol Experience

 Subsurface Camera Using Amphenol Waterproof Connectors and a Watertight Hammond Manufacturing Enclosure 

 Experimenting with Waterproof Connectors 

 Experimenting With Waterproof Connectors 

  • Sign in to reply
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    I'm guessing that someone is about to add golf to the list of sports they play ?

    Looks like a divot tool / ball marker, however if the green is under that amount of water, I think it is perhaps time to put it away and retire to the 19th hole.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to beacon_dave

    Maybe a contraption like this could be used to find golf balls in water hazards....Relaxed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to dougw

    You might need an airlock to get the recovered balls into the enclosure without flooding the camera Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 3 years ago in reply to dougw

    You might need an airlock to get the recovered balls into the enclosure without flooding the camera Slight smile

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to beacon_dave

    After watching a video of a YouTuber collecting around 2000 golf balls from a single water hazard, I think you might need to consider a slightly larger enclosure...  Slight smile

    Either that or time to dust off the SCUBA gear...