Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Enclosure IP rating confusion
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 36 subscribers
  • Views 3405 views
  • Users 0 members are here
  • waterproof connectors
Related

Enclosure IP rating confusion

JWx
JWx over 3 years ago

Hello!

after briefly studying enclosure datasheet I have found something strange: it is described as IP68 (NEMA 4, 4X, 6, 6P, 12, 13), but PDF provided

www.farnell.com/.../2239464.pdf

states only: NEMA 4, 4X

in addition, family description from manufacturer's site:

https://www.hammfg.com/electronics/small-case/plastic/1554

states that this family is "NEMA Type 4, 4X, 6, 6P, 12 & 13", "Except 1554/55 V size which is 4,4X only"

as there are a few part numbers with V inside (VGY, VALGY, VAGY, VBGY) I wonder if our enclosure (1554VA2GYCL) can be considered IP68 or NEMA4X (so no submersion allowed)?

  • Sign in to reply
  • Cancel

Top Replies

  • charlieo21
    charlieo21 over 3 years ago +3 verified
    I had a little chat with a Hammond Technical Product Specialist. She confirmed that our enclosure meets IP68.
  • ralphjy
    ralphjy over 3 years ago +1
    I saw that also. I had planned on a submersion test, but submersion is not required for my application. I would expect that since most of the enclosures have an IP68 rating, that it should meet the temporary…
  • dougw
    dougw over 3 years ago +1
    I think the statement that V size is only rated for Nema 4 (IP65) applies to this enclosure. I will be using it in an immersion application anyway and hopefully taking enough precautions to ensure the…
Parents
  • ralphjy
    0 ralphjy over 3 years ago

    I saw that also.  I had planned on a submersion test, but submersion is not required for my application.  I would expect that since most of the enclosures have an IP68 rating, that it should meet the temporary (30 min) submersion requirement.  Not sure how to interpret the spec - does the NEMA 4 indicate that it failed NEMA 6 or that it wasn't tested?  It would be nice if they provided the IP rating for this specific enclosure if it is different.

    The Amphenol connectors are also only rated to IP67 and at least one (4p circular) is only rated when mated.  I think the challenge will be using the connectors when submerged.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ralphjy
    0 ralphjy over 3 years ago

    I saw that also.  I had planned on a submersion test, but submersion is not required for my application.  I would expect that since most of the enclosures have an IP68 rating, that it should meet the temporary (30 min) submersion requirement.  Not sure how to interpret the spec - does the NEMA 4 indicate that it failed NEMA 6 or that it wasn't tested?  It would be nice if they provided the IP rating for this specific enclosure if it is different.

    The Amphenol connectors are also only rated to IP67 and at least one (4p circular) is only rated when mated.  I think the challenge will be using the connectors when submerged.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • JWx
    0 JWx over 3 years ago in reply to ralphjy

    When clicking specific parts on manufacturer's portal our enclosure P/N is reported as IP68, but - for example - 1554V2GYCL (the same size but with 4 screws, not 6 as in our model) is only IP66.

    Maybe cover of this size when secured only with 4 screws is failing NEMA6? I think lack of NEMA6 is because of test failure - in my opinion manufacturer would test the whole family (it adds value after all) and exclude only models that have failed specific tests...