Experimenting with Waterproof Connectors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Waterproof Connectors
  • More
  • Cancel
Experimenting with Waterproof Connectors
Experimenting with Waterproof Connectors Forum Enclosure IP rating confusion
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Experimenting with Waterproof Connectors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 36 subscribers
  • Views 3485 views
  • Users 0 members are here
  • waterproof connectors
Related

Enclosure IP rating confusion

JWx
JWx over 3 years ago

Hello!

after briefly studying enclosure datasheet I have found something strange: it is described as IP68 (NEMA 4, 4X, 6, 6P, 12, 13), but PDF provided

www.farnell.com/.../2239464.pdf

states only: NEMA 4, 4X

in addition, family description from manufacturer's site:

https://www.hammfg.com/electronics/small-case/plastic/1554

states that this family is "NEMA Type 4, 4X, 6, 6P, 12 & 13", "Except 1554/55 V size which is 4,4X only"

as there are a few part numbers with V inside (VGY, VALGY, VAGY, VBGY) I wonder if our enclosure (1554VA2GYCL) can be considered IP68 or NEMA4X (so no submersion allowed)?

  • Sign in to reply
  • Cancel

Top Replies

  • charlieo21
    charlieo21 over 3 years ago +3 verified
    I had a little chat with a Hammond Technical Product Specialist. She confirmed that our enclosure meets IP68.
  • ralphjy
    ralphjy over 3 years ago +1
    I saw that also. I had planned on a submersion test, but submersion is not required for my application. I would expect that since most of the enclosures have an IP68 rating, that it should meet the temporary…
  • dougw
    dougw over 3 years ago +1
    I think the statement that V size is only rated for Nema 4 (IP65) applies to this enclosure. I will be using it in an immersion application anyway and hopefully taking enough precautions to ensure the…
Parents
  • dougw
    0 dougw over 3 years ago

    I think the statement that V size is only rated for Nema 4 (IP65) applies to this enclosure. I will be using it in an immersion application anyway and hopefully  taking enough precautions to ensure the project works. (a minor leak won't cause failure) It should be interesting to see how well it performs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 3 years ago

    I think the statement that V size is only rated for Nema 4 (IP65) applies to this enclosure. I will be using it in an immersion application anyway and hopefully  taking enough precautions to ensure the project works. (a minor leak won't cause failure) It should be interesting to see how well it performs.