Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum RDM3600 RFID COMPONENT
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 8 subscribers
  • Views 4585 views
  • Users 0 members are here
Related

RDM3600 RFID COMPONENT

e14 Contributor
e14 Contributor over 11 years ago

I have been using the Arduino platform for a while now(about 6 months) and I tried to hook up the RDM3600 RFID reader to my Arduino Uno and it seems like the reader does not communicate with the board. I present a card, but the serial interface does not display a serial number or anything. I am following this tutorial:

 

http://tronixstuff.com/2013/11/19/arduino-tutorials-chapter-15-rfid/

 

I modified the code to get an indication that the setup was complete:

 

#include <SoftwareSerial.h>

 

SoftwareSerial RFID(2, 3);

 

int i;

 

void setup()

{

  RFID.begin(9600);

  Serial.begin(9600);

  Serial.println("ready");

}

 

void loop()

{

  if (RFID.available() > 0)

  {

    i=RFID.read();

    Serial.print(i, DEC);

    Serial.println(" next");

  }

}

 

 

 

Does anyone have any idea why I don't get any communication from the RDM3600 when I present a RFID tag.

  • Sign in to reply
  • Cancel
Parents
  • kgenskowsky
    0 kgenskowsky over 11 years ago

    Hi There,

     

    You can always use a RS232 converter to connect the module to a PC serial port and check that the module is working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kgenskowsky
    0 kgenskowsky over 11 years ago

    Hi There,

     

    You can always use a RS232 converter to connect the module to a PC serial port and check that the module is working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kgenskowsky

    Kevin, I'm not sure this computer has a serial port. I only see USB.