Design Challenges
  • Challenges & Projects
  • More
Design Challenges
Forum RDM3600 RFID COMPONENT
  • Blogs
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 29 replies
  • Subscribers 8 subscribers
  • Views 4813 views
  • Users 0 members are here
Related

RDM3600 RFID COMPONENT

e14 Contributor
e14 Contributor over 11 years ago

I have been using the Arduino platform for a while now(about 6 months) and I tried to hook up the RDM3600 RFID reader to my Arduino Uno and it seems like the reader does not communicate with the board. I present a card, but the serial interface does not display a serial number or anything. I am following this tutorial:

 

http://tronixstuff.com/2013/11/19/arduino-tutorials-chapter-15-rfid/

 

I modified the code to get an indication that the setup was complete:

 

#include <SoftwareSerial.h>

 

SoftwareSerial RFID(2, 3);

 

int i;

 

void setup()

{

  RFID.begin(9600);

  Serial.begin(9600);

  Serial.println("ready");

}

 

void loop()

{

  if (RFID.available() > 0)

  {

    i=RFID.read();

    Serial.print(i, DEC);

    Serial.println(" next");

  }

}

 

 

 

Does anyone have any idea why I don't get any communication from the RDM3600 when I present a RFID tag.

  • Sign in to reply
  • Cancel
Parents
  • kgenskowsky
    0 kgenskowsky over 11 years ago

    Hi There,

     

    You can always use a RS232 converter to connect the module to a PC serial port and check that the module is working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kgenskowsky

    Kevin, I'm not sure this computer has a serial port. I only see USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to kgenskowsky

    Kevin, I'm not sure this computer has a serial port. I only see USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to e14 Contributor

    kgenskowsky is right. You could connect the module directly to your computer.

     

    It is very common for computers to omit the Serial Port these days. You could use a cable similar to the one I linked-to earlier, and connect that to a USB port. The cable I suggested works on TTL level so there would be no logic level conversion required.

     

    The tag you linked to is an NFC tag that works on 13.56MHz, so if you want to continue using those tags you may need to look at alternative readers.

    I have one of these: SainSmart Mifare RC522 Card Read Antenna RF RFID Reader IC Card Proximity Module 3D Printing, Arduino, Robotics | Sainsm… modules that works on the frequency required but I haven't tested it yet. They are available from many places online.

    There is an article about increasing the range od these modules here: Extend range for MFRC522 RFID Reader