Forget Me Not Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Forget Me Not Design Challenge
  • More
  • Cancel
Forget Me Not Design Challenge
Blog [CaTS] ForgetMeNot - Week 1: EnOceanPi and Sensors
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fvan
  • Date Created: 1 Aug 2014 1:47 PM Date Created
  • Views 4260 views
  • Likes 6 likes
  • Comments 19 comments
  • forget_me_not
  • design_challenge
  • openhab
  • tektronix
  • iot_pet_care
  • eclipse
  • internet_of_things
  • enocean
  • cats
  • raspberrypi
  • smarthome
  • challenge
  • iot
  • enocean_pi
Related
Recommended

[CaTS] ForgetMeNot - Week 1: EnOceanPi and Sensors

fvan
fvan
1 Aug 2014

Previous posts for this project:

  • [CaTS] ForgetMeNot - Index
  • [CaTS] ForgetMeNot - Week 0: Project Description

 

  • Introduction
  • Setting Up RaspberryPi
  • Setting Up EnOceanPi
    • Sensor IDs
  • Setting Up OpenHAB
    • Core
    • Bindings
    • Demo
    • Running
    • Exploring
    • Designer
    • iOS App
  • RaspberryPi + EnOcean + OpenHAB
  • Start at boot

 

Introduction

 

Last week, I described the project I intend to realise for this challenge.

 

Now, I have started experimenting with openHAB in combination with the Raspberry Pi B+ and the EnOcean sensor kit.

This post will cover the steps needed to get a basic openHAB configuration running with the sensors.

 

Setting Up RaspberryPi

 

I set up my Pi using the latest Wheezy image available from the RaspberryPi website.

You can find a step-by-step guide from shabaz here: Raspberry Pi Setup Guide

 

After the Pi booted, I configured the typical things I use with the raspi-config tool:

  • expand file system
  • enable ssh
  • update

 

Once that was done, I powered off the Pi and connected the EnOceanPi module before powering on again.

imageimage

 

 

Setting Up EnOceanPi

 

Knowing the EnOceanPi and Sensors were Roadtested not so long ago, I browsed the reviews to read on their experiences.

This was particularly useful to know which problems they faced to get the sensors up and running.

 

malakai's EnOcean review provided a few simple commands to set everything up:

 

pi@webserver ~ $ sudo wget https://raw.github.com/lurch/rpi-serial-console/master/rpi-serial-console -O /usr/bin/rpi-serial-console && sudo chmod +x /usr/bin/rpi-serial-console
--2014-07-09 10:24:02--  https://raw.github.com/lurch/rpi-serial-console/master/rpi-serial-console
Resolving raw.github.com (raw.github.com)... 23.235.43.133
Connecting to raw.github.com (raw.github.com)|23.235.43.133|:443... connected.
HTTP request sent, awaiting response... 301 Moved Permanently
Location: https://raw.githubusercontent.com/lurch/rpi-serial-console/master/rpi-serial-console [following]
--2014-07-09 10:24:07--  https://raw.githubusercontent.com/lurch/rpi-serial-console/master/rpi-serial-console
Resolving raw.githubusercontent.com (raw.githubusercontent.com)... 23.235.43.133
Connecting to raw.githubusercontent.com (raw.githubusercontent.com)|23.235.43.133|:443... connected.
HTTP request sent, awaiting response... 200 OK
Length: 2829 (2.8K) [text/plain]
Saving to: `/usr/bin/rpi-serial-console'


100%[==============================================================================================>] 2,829       --.-K/s   in 0.001s


2014-07-09 10:24:11 (3.29 MB/s) - `/usr/bin/rpi-serial-console' saved [2829/2829]

 

 

Execute the script to disable the serial console, allowing it to be used by other programs:

 

# Script by AndrewS to make it easier to enable/disable the serial console
# (which allows the UART to be used by other programs)
# version 1.1 - better error handling

 

pi@webserver ~ $ sudo rpi-serial-console disable
Serial console has been disabled, a reboot is required to make this take effect

 

 

Reboot the Pi to apply the changes to the serial console:

 

pi@webserver ~ $ sudo reboot

Broadcast message from root@webserver (pts/0) (Wed Jul  9 10:28:09 2014):

The system is going down for reboot NOW!

 

Sensor IDs

 

To be able to use the sensors in openHAB, their unique ID is required.

 

To do this, I've installed FHEM, which auto-detects the IDs, wrote them down and disabled FHEM again.

Installing and using FHEM is also covered in the Road Test review linked earlier.

 

I haven't found an easier way to do this (yet).

 

 

Setting Up OpenHAB

 

There is a simple installation procedure on the OpenHAB website: openHAB - empowering the smart home

Following the instructions, and with a bit of common sense, installation went smoothly.

 

Core

 

First step is to install the OpenHAB core software. this is easily done by extracting the proper zip file to the correct location on the Pi:

 

pi@webserver ~ $ sudo mkdir /opt/openhab
pi@webserver ~ $ cd /opt/openhab/
pi@webserver /opt/openhab $ sudo unzip /home/pi/distribution-1.5.0-runtime.zip

 

 

Bindings

 

Next step is to add some bindings by extracting the addons zip file in the addons folder. This will however deploy *all* addons.

Once deployed, you can remove the addons which are not required by removing the correct *.jar files.

 

pi@webserver /opt/openhab $ cd addons/
pi@webserver /opt/openhab/addons $ sudo unzip /home/pi/distribution-1.5.0-addons.zip
pi@webserver /opt/openhab/addons $ cd ..
pi@webserver /opt/openhab $ sudo cp configurations/openhab_default.cfg configurations/openhab.cfg

 

 

Demo

 

There is a demo app available. In order to get to know the different components of an app, I deployed it:

 

pi@webserver /opt/openhab $ sudo unzip /home/pi/distribution-1.5.0-demo-configuration.zip

 

 

Running

 

With all OpenHAB components deployed, it was time to start it up. I noticed the "start.sh" script was not executable by default, so I updated that.

 

pi@webserver /opt/openhab $ sudo chmod +x start.sh
pi@webserver /opt/openhab $ sudo ./start.sh

 

 

Exploring

 

With the demo installed and started, I crossed my fingers and accessed the OpenHAB interface: http://192.168.0.205:8080/openhab.app?sitemap=demo

 

It works! The demo is up and running and there are various examples of widgets, multimedia, etc ... to browse:

 

imageimage

 

Designer

 

Next I decided to install the designer on my Mac.

 

After launching the Designer, the program would just get stuck on the splash screen and nothing would happen.

I Googled a bit a came across this thread: https://code.google.com/p/openhab/issues/detail?id=439

 

As mentioned in one of the comments, I added a line to my openHAB-Designer.ini file:

 

-Djava.awt.headless=true

 

The designer now launches properly.

image

 

With the designer running on my Mac and the Core running on the Pi, I wanted an easy way to develop and deploy new OpenHAB configurations.

To do that, I defined a password for user "root", installed samba and shared the OpenHAB folder.

 

pi@webserver /opt/openhab $ sudo passwd root

 

pi@webserver /opt/openhab $ sudo apt-get install samba samba-common-bin

 

pi@webserver /opt/openhab $ sudo nano /etc/samba/smb.conf

 

[openhab]
   comment=OpenHAB
   path=/opt/openhab
   browseable=Yes
   writeable=Yes
   only guest=no
   create mask=0777
   directory mask=0777
   public=no

 

pi@webserver /opt/openhab $ sudo smbpasswd -a root

 

On my Mac, I mounted the shared folder and got access to the OpenHAB installation on the Pi:

imageimage

 

From the designer, I could now load the OpenHAB config and access the demo:

image

 

iOS App

 

Finally, I installed the OpenHAB app on my smartphone and pointed it to the Raspberry Pi, by:

  • specifying the remote url: http://192.168.0.205:8080/openhab.app
  • setting demo mode to off

 

imageimage

 

RaspberryPi + EnOcean + OpenHAB

 

With all parts individually set up, I tried combining everything to a working solution.

 

Following the documentation found at https://github.com/openhab/openhab/wiki/EnOcean-Binding, I configured the serial port of my EnOceanPi in the openhab.cfg:

 

################################# EnOcean Binding #####################################
#
# EnOcean USB adapter serial port
enocean:serialPort=/dev/ttyAMA0

 

After the modification, I restarted OpenHAB and started modifying the demo example to have my EnOcean switch and temperature sensor available.

 

First, I edited the "demo.items" file to contain the following:

 

Switch EnOcean_switch_00298B1A {enocean="{id=00:29:8B:1A, eep=F6:02:01, channel=B}"}
Number EnOcean_sensor_01809DC1 "Temperature [%.1f °C]" <temperature> (enocean) {enocean="{id=01:80:9D:C1, eep=A5:02:05, parameter=TEMPERATURE}"}
Contact EnOcean_sensor_0180878B "Contact [MAP(en.map):%s]" <contact> (enocean) {enocean="{id=01:80:87:8B, eep=D5:00:01, parameter=CONTACT_STATE"}


I continued by updating the "demo.sitemap" to only visualise those three items:


sitemap demo label="Main Menu"
{
 Frame label="EnOcean" {
  Switch item=EnOcean_switch_00298B1A label="Switch"
  Text item=EnOcean_sensor_01809DC1 valuecolor=[>25="orange",>15="green",>5="orange",<=5="blue"]
  Text item=EnOcean_sensor_0180878B
  }
}

 

With everything configured, I started clicking my EnOcean switch like a madman. Nothing happened.

 

After searching for quite some time, I found I needed to make a modification to the OpenHAB "start.sh" script in order to recognise the serial port.

 

I edited "start.sh" as mentioned in this thread: https://groups.google.com/forum/#!searchin/openhab/enocean/openhab/8GtLqJAffcI/zJ1DGF95XOsJ

 

-Dgnu.io.rxtx.SerialPorts=/dev/ttyAMA0

 

Restarted OpenHAB and guess what? It worked!

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image
image

 

This is already a great step forward!

 

 

Start at boot

 

To finalise this week's post, I ensured openHAB would start automatically when booting the Pi.

 

To do this, I edited "/etc/rc.local" and added this line:

 

sudo /opt/openhab/start.sh

 

To test this, I rebooted the Pi, and openHAB started automatically!

  • Sign in to reply

Top Comments

  • ravi_butani
    ravi_butani over 12 years ago +1
    Wow!!!! really good blog post... about setup openHAB and EnOcean too... It will be very helpful for others.....
  • fvan
    fvan over 12 years ago in reply to ravi_butani +1
    Thanks! This might be a competition, but we'll learn even more (from each other) if we all manage to move forward with our project and document/share our experiences!
  • fvan
    fvan over 12 years ago in reply to ravi_butani +1
    Sounds strange that enabling the camera module would help to get openhab started, but if it works, it works
  • fvan
    fvan over 12 years ago in reply to ravi_butani

    Sounds strange that enabling the camera module would help to get openhab started, but if it works, it works image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to ravi_butani

    Ravi;

    When I first went through the instructions from openHAB I did everything they said, but I could not get the system to load. I thought about it for a while, and I realized I was not starting the openHAB server in super user mode image. After I changed that, everything started working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ravi_butani
    ravi_butani over 12 years ago in reply to fvan

    I have tried all the day and night but no luck... Then from raspi-config i have eneble camera module then BINGO!!!!! openHAB demo start working without any issue.... I dont know how it was on track but its doneimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 12 years ago in reply to ravi_butani

    Can you post the full stack trace ? Which bindings and add-ons have you deployed ?

     

    I would propose that in the "addons" folder you remove all the bindings etc that you don't use.

    In my case there are only a couple of files:

    • org.openhab.binding.exec
    • org.openhab.binding.enocean
    • org.openhab.persistence.mysql

     

    I moved all the other *.jar files to a subfolder for future use.

     

    Note: openhab should start just fine with all add-ons loaded, but only loading the ones you need is more efficient.

     

    Frederick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ravi_butani
    ravi_butani over 12 years ago

    Hi @Frederick, I am facing problem in setup openHAB on rasi-Pi B I am using latest Rasbian-Wheezy os. I am following same steps you have mentioned but no luck... do i need to install java or any thing else..? As I have seen that latest raspbian os comes with java jdk 7... do i need to enable it? error is ERROR o.o.m.c.i.f.FolderObserver[:105] - An unexpected exception has occured

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>