In the Air Design Challenge
  • Challenges & Projects
  • Design Challenges
  • In the Air Design Challenge
  • More
  • Cancel
In the Air Design Challenge
Blog AirMobile - Description
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
  • Author Author: amgalbu
  • Date Created: 3 Nov 2014 7:38 AM Date Created
  • Views 1357 views
  • Likes 2 likes
  • Comments 6 comments
  • iot_distributed
  • in_the_air
Related
Recommended

AirMobile - Description

amgalbu
amgalbu
3 Nov 2014

Abstract

This is a proposal for a distributed network of air quality sensors. In this document, I will write down details for making a sensor that can be installed on cars, but in the future handlebar-mounted and armband versions of the sensor can be designed.

The sensor is battery-free and harvest energy from car radiator heat by means of a Peltier cell. Data is transferred to a smartphone through a Bluetooth Low Energy link. The smartphone internet connectivity is leveraged to push data to a cloud service.

Data from all the installed sensors can be analyzed at home thanks to a plugin that will be developed as part of this project. Plugin will pull data from the cloud and make automation decisions thanks to the power and flexibility of the OpenHAB platform

Architecture overview

 

image

 

Figure 1 - System architecture

 

Sensor

The air quality sensor is made of the following main components

  1. 1.      a low-power microcontroller, like the Texas Instruments MSP430 series microcontroller
  2. 2.      a Bluetooth Low Energy module, like the Texas Instruments LMX5252 module
  3. 3.      a dust sensor module, like the Sharp GP2Y1010AU0F, which features a low power consumption
  4. 4.      a N02 sensor, like the MiCS 2710 NO2 gas Sensor
  5. 5.      a C0 sensor, like the Figaro TGS 2442 CO gas sensor
  6. 6.      a humidity sensor
  7. 7.      a temperature sensor
  8. 8.      a Peltier element for energy harvesting. The use of energy harvesting makes the sensor installation absolutely unobstrusive

 

image

Figure 2 - Sensor schematic

 

 

image

Figure 3- Sensor electrical components and connections

 

Sensor will be enclose in a box designed to be easily fixed to the radiator grid

 

image

Figure 4 - Sensor case rendering

 

 

image

Figure 5 - Mounting position

 

 

 

 

Smartphone runs an application that

  1. 1.      pushes data to the cloud
  2. 2.      shows sensor current readings
  3. 3.      show sensor readings history

 

There are other products (like the Air Quality Egg) that make air quality data available on the cloud, so it would be advisable that data coming from car sensors contribute to enrich the amount of information available is these repositories instead of creating a new one

 

Data fusion

At home, a BeagleBone board runs OpenHAB gathers data from the cloud infrastructure by means of a plugin developed as a part of this project. The plugin leverage web API to read data from the cloud. Data will then be available in the OpenHAB platform and processed using all the facilities available in such a powerful automation system.

The OpenHAB could also get additional information from other sources to enrich air quality data. For example, reading

  • weather data
  • forecasts
  • air quality measurements provided by fixed stations and from the Air Quality Egg project devices

 

can help select the best time of day when an outdoor training session is advisable because both weather and air quality are good. Note that it is possible to detect time-dependant trends in the air quality. For example, air quality is likely to get worse during rush hours

With OpenHAB automation mechanism, user can get a tweet when air quality is good enough to have some outdoor training or suggest that it's better to stay at home (in that cause ventilators could be switched off to prevent polluted air from entering the house)

Thanks to air quality maps, a family could also plan the path with the best air quality for the Sunday bike trip with the children.

  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago in reply to tomaja +1
    Hi Dragan Yes, the idea is to geolocalize data by levergaing the smartphone GPS Ambrogio
  • tomaja
    tomaja over 11 years ago in reply to nikil511 +1
    Yes, and if you publish your findings that green one would soon turn red
Parents
  • tomaja
    tomaja over 11 years ago

    Good idea!

    Have you considered adding the GPS support? This would allow you to make an interesting map if you are often on the road (car or bicycle).

     

    Dragan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja

    Hi Dragan   

    Yes, the idea is to geolocalize data by levergaing the smartphone GPS

     

    Ambrogio

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • amgalbu
    amgalbu over 11 years ago in reply to tomaja

    Hi Dragan   

    Yes, the idea is to geolocalize data by levergaing the smartphone GPS

     

    Ambrogio